cancel
Showing results for 
Search instead for 
Did you mean: 

Write protection WRP section disappeared from OB between 2.15 and 2.17

jmull
Associate II

It seems the write protection section has disappeared from the CubeMX programmer some time between versions 2.15 and 2.17?  It is not visible in the UI or the CLI.  We are having trouble programming our boards without access to this section.

1 ACCEPTED SOLUTION

Accepted Solutions
Aziz BRIGUI
ST Employee

Hello @jmull,

Issue is fixed in the newest STM32CubeProgrammer release available under this link.

Aziz


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

8 REPLIES 8
STTwo-32
ST Employee

Hello @jmull and welcome to the ST Community 

Could you please add more details (what board/MCU are you using?). 

PS: It is Cube Programmer and not CubeMX Programmer.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

jmull
Associate II

Yes it is a custom board with the STM32G491CCUx.  I'm using the ST-Link v2 to connect.

liaifat85
Senior III

If the GUI doesn’t display the option, the CLI may still support write protection commands.

Try this command:

STM32_Programmer_CLI -c port=SWD -wprotect enable [address] [sector]

Thanks liaifat85.  I've rolled back to 2.15 so I can't try that at the moment but I can say it didn't appear when I did

STM32_Programmer_CLI.exe -c port=swd -ob displ

Hello @jmull 

Can you send some screenshots showing the issue. I'm not able to reproduce this issue using the Nucleo-G491RE.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Aziz BRIGUI
ST Employee

Hello @jmull,

This is a known issue and tracked internally in Ticket 189999. It will be fixed in a future release.

Aziz 


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Cheers Aziz

Aziz BRIGUI
ST Employee

Hello @jmull,

Issue is fixed in the newest STM32CubeProgrammer release available under this link.

Aziz


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.