2020-10-07 02:29 AM
17:23:22 : Address : 0x00000224
17:23:22 : Erasing memory corresponding to segment 0:
17:23:22 : Erasing memory corresponding to segment 1:
17:23:22 : Erasing internal memory sector 0
17:23:22 : Erasing memory corresponding to segment 2:
17:23:22 : Erasing internal memory sectors [0 10]
17:23:22 : Erasing memory corresponding to segment 3:
17:23:22 : Erasing internal memory sector 32
17:23:22 : Erasing memory corresponding to segment 4:
17:23:22 : Erasing internal memory sectors [32 57]
17:23:23 : Download in Progress:
17:23:23 : Error: failed to download Segment[0]
17:23:23 : Error: failed to download the File
2020-10-08 03:42 AM
Hi @CCai.1
Could you please share your .bin file to check with.
Best regards,
Nesrine
2020-10-09 12:09 AM
2020-10-09 07:23 AM
Hi @CCai.1
Tested the same scenario by using my own .bin i had no issue.
14:59:35:602 : Download in Progress:
14:59:35:603 : Size : 262144 Bytes
14:59:35:603 : Address : 0x08000000
14:59:35:603 : Buffer program...
14:59:35:607 : halt ap 0
14:59:35:608 : w ap 0 reg 15 PC (0x20000000)
14:59:35:609 : w ap 0 reg 17 MSP (0x20000500)
14:59:35:610 : w ap 0 reg 16 xPSR (0x01000000)
14:59:35:612 : w ap 0 @0x20000860 0x00000200 bytes Data 0x00000000
14:59:35:612 : w ap 0 @0x20000000 0x00000004 bytes Data 0x0000BE00
14:59:35:614 : w ap 0 @0x20000004 0x00000430 bytes Data 0xF000B580
14:59:35:615 : Loader write range...
14:59:35:697 : w ap 0 @0x20000860 0x00003A00 bytes Data 0x20200408
14:59:35:697 : W B1 in RAM @0x20000860 size 0x00003A00 : 0098ms
14:59:35:697 : Init flashloader...
But when i test with your .bin i get an error when downloading:
5:01:05:303 : Download in Progress:
15:01:05:303 : Size : 8 Bytes
15:01:05:303 : Address : 0x00000224
15:01:05:303 : Buffer program...
15:01:05:303 : w ap 0 @0x00000224 0x00000008 bytes Data 0x000051F1
I think the problem is with your code, so please try to check the linker ( address w segments)
Best regards,
Nesrine