cancel
Showing results for 
Search instead for 
Did you mean: 

When flashing firmware, the characters are garbled

totoro
Associate II

Hi, thank you for having access to this report.

Here is STM32CubeProgrammer's output text.

(0) > STM32_Programmer_CLI --connect port=swd -w .\board\art-pi\projects\applications\build\Debug\applications.elf 0x90000000 -v -el .\board\art-pi\ExternalLoader\ART-Pi_W25Q64.stldr ------------------------------------------------------------------- STM32CubeProgrammer v2.17.0 ------------------------------------------------------------------- ST-LINK SN : 066BFF554957886687101038 ST-LINK FW : V2J42M27 Board : -- Voltage : 3.27V SWD freq : 4000 KHz Connect mode: Normal Reset mode : Software reset Device ID : 0x450 Revision ID : Rev V Device name : STM32H7xx Flash size : 128 KBytes Device type : MCU Device CPU : Cortex-M7 BL Version : 0x91 Warning: Write address is ignored for hex, Srec, s19 and elf files Memory Programming ... Opening and parsing file: applications.elf File : applications.elf Size : 996.35 KB Address : 0x90000000 Erasing memory corresponding to segment 0: Erasing external memory sectors [0 249] Download in Progress: ��������������������������������������������������� 100% File download complete Time elapsed during download operation: 00:00:11.568 Verifying ... Read progress: ��������������������������������������������������� 100% Download verified successfully
View more

This works fine, but he doesn't feel very well.

And I tried to use utf-8 encoding format, but it's still garbled.

 

11 REPLIES 11
Aziz BRIGUI
ST Employee

Hello @totoro

I don't think this is a bug since STM32_Programmer_CLI is normally used in cmd shell on Windows or Terminals on MAC or Linux (With the default encoding (IBM850), the progress bar is displayed as expected).

Could you specify what you're using exactly ?

As I see it, this is most certainly a Terminal encoding issue. Could you try the following : 

>chcp 850

 

Let me know if it solves the issue,

Aziz


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Aziz BRIGUI
ST Employee

Hello @totoro

Did my previous comment resolve the issue ? If yes, could you please accept the answer as solution so that it could easily be found by other users ?

Thanks in advance,

Aziz


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

@Aziz BRIGUI wrote:

mark the answer as best


Note that the option now appears as 'Accept as Solution' rather than "best":

AndrewNeil_0-1729696530922.png

https://community.st.com/t5/feedback-forum/need-an-other-tools-section/td-p/734522

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Hi @Andrew Neil

Yes, old habit from the old platform.

Comment edited accordingly,

Thanks a lot,

Aziz


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Sorry, I forgot to reply, this method cannot solve that problem.123.jpg

I agree with @Aziz BRIGUI - the problem there is the configuration of your terminal: it's not correctly displaying the graphic characters used by CubeProgrammer to display the progress bar.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

I think I understand. It may be related to one of my settings.

totoro_0-1729757662716.png

 

So what happens if you change that?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

It still does not display the progress bar's graphic characters correctly, but the result is different from before.capture_20241025215202748.jpg