cancel
Showing results for 
Search instead for 
Did you mean: 

using SPI protocol multi-slave modules with master stm32f1

Hg.1
Associate

Hello there,

I am working on a project. In the project I want to implement, an external ADC module will collect the data and transfer it to the STM32F103C8. My STM32F103C8 microprocessor will transfer these data to my wireless module. Here I am having trouble with SPI communication. Using SPI1, the STM32F103C8 will be the master, while my other two modules will work as slaves. How can I compile this using single SPI?

1 REPLY 1
TDK
Guru

Duplicate:

https://community.st.com/s/question/0D53W00001B0yPdSAJ

No need to post with different tags. You can add tags if you want.

If you feel a post has answered your question, please click "Accept as Solution".