Use STM32CubeProgrammer API will show Error: Device not supported
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-05-31 5:46 AM
Hi All
My customer try to use STM32CubeProgrammer API, when run the UART Bootloader Example will show "Error: Device not supported",
How to fixed this issue?
Hardware platform: NUCLEO-G070RB
STM32Cubeprogrammer API version: 2.1.0
As below is log file content.
STM32CubeProgrammer API v2.1.0
+++ UART Bootloader Example +++
------------- Serial Port List --------------
Port Name [0] : COM3
Port Name [1] : COM5
---------------------------------------------
Serial Port COM5 is successfully opened.
Port configuration: parity = even, baudrate = 115200, data-bit = 8,
stop-bit = 1.0, flow-control = off
QObject::startTimer: Timers can only be used with threads started with QThread
Activating device: OK
Chip ID: 0x460
BootLoader protocol version: 3.1
Error: Device not supported
- Labels:
-
STM32CubeProgrammer