cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to connect (& hence flash the firmware) the STM32-Cube-Programmer with STM32-target-board in USB-DFU-mode if loaded firmware is read-protected.

nirav soni
Associate II

1) I am able to connect the STM32-Cube-Programmer in USB-DFU-mode if existing or loaded firmware in to STM32-target-board is not read-protected.

Image-1: Able to connect with target board

0690X000009Z7piQAC.png

Image-2: Able to load firmware in to target board

0690X000009Z7qWQAS.png

2) I am not able to connect the STM32-Cube-Programmer in USB-DFU-mode if existing or loaded firmware in to STM32-target-board is read-protected.

Image-3: Not even able to connect with target board0690X000009Z7rUQAS.png

In this case I am keep getting the DFU connection error,

How to resolve this application bug.

Programmer seems to be not professionally viable,

Has anyone in community found resolution to this application bug.

Can anybody in STM comment?

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
SBone.3
Associate II

Hi, i opened another thread about this topic, also providing them USB traces to debug the issue but i haven't received an answer yet.

https://community.st.com/s/question/0D53W00001ddlkLSAQ/bug-stm32cubeprogrammer-usb-connection-to-stm32-bootloader-device-fails

you can try to comment there as well, to solicit them for a response..