cancel
Showing results for 
Search instead for 
Did you mean: 

Tried to download the Atollic ELF file via STM32 Cube programmer. "download failed" Converted to hex and tried to download. "Download failed". Why I can't download hex files produced by Atollic?

Ggast
Associate III
7 REPLIES 7

Without knowing the part, or seeing the ELF/HEX file, I'd have to assume you've built the code for the wrong address.

Can STM32 Cube Programmer read the part? Save a .HEX file? Load/write that .HEX file?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Ggast
Associate III

Its Nucleo H743ZI.

Address FACEBOOC a joke?

0690X000008AsGVQA0.jpg

>>Address FACEBOOC a joke?

Probably to someone. @Nawres GHARBI​ 

Seems to load in v1.1.0 Ok might look at an NUCLEO-H743ZI with a newer build later if I have time.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Nawres GHARBI
ST Employee

Hi @Ggast​ 

Could you attach the .elf or .out please ?

If fact this not a joke, 0xFACEB00C is used to init a pointer with a dummy value for debug stuff.

We used this value to catch a bug, so it will be helpful to have your .elf

The Unix coders had more humor, and used 0xDEADBEEF.

That's an OS these millennials grandparents wrote.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Ah, thanks for the explanation ... :)