cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7B3I-DK, Error message from debugger back end: Load failed

IChoi.2
Associate

Hi All,

Board : STM32H7B3I-DK

IDE : STM32CubeIDE 10.1

I'm trying to download demo app from STM32CubeIDE.

The demo apps are AudioPlayer and FreeRTOS from "Example Selector".

The building is done, but I'm getting an error as Run.

0693W00000QM8ZHQA1.jpg 

But I can load en.STM32H7B3I-DK_Demo to use the STM32CubeProgrammer.

How to run some demo app in STM32CubeIDE?

2 REPLIES 2
ChahinezC
Lead

Hello @IChoi.2​,

It seems the issue you are facing is similar to the one reported in this thread.

I hope Semer's answer helps you solve your problem.

If this solves your problem, please mark my answer as "Best Answer" by clicking on the "Select as Best" button, this can be very helpful for Community users to find this solution faster.

Thank you.

Chahinez.

Could the error reporting perhaps be less cryptic and more specific about what actually failed.

B​uild suggest external SDRAM, is that some thing that has an external loader, or debug script?

S​TM32 Cube Programmer supposedly works on same ELF, so exists, is that using an external loader?

Directory name has odd Japanese double bytes.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..