cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G431 connect over JTAG

CHeck.1
Associate II

Hello,

I try to connect to a STM32G431 Device over JTAG. I got the following error. Has someone a solution for this error?

0693W000006GEUkQAO.png

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
KnarfB
Super User

Did you upgrade to the latest tool version like STM32CuberProgrammer 2.6?

CHeck.1
Associate II

Yes I am using V2.6

KnarfB
Super User

Custom board? Nucleo32 works here as expected. What probe?

CHeck.1
Associate II

It is a self developed board. The JTAG connection works with an J-Link but not the ST-Link and STM32CubeProgrammer. Just a connection over SWD

KnarfB
Super User

Communication errors? You can lower the clock speed and re-check.

Uwe Bonnes
Principal III

Firmware on the STLink recent? All STlink match JTAG ID against an internal list and reject parts they do not know(yet).

CHeck.1
Associate II

Firmware on ST Link is recent

Uwe Bonnes
Principal III

Does connect under reset work?

CHeck.1
Associate II

No, it doesn't work