cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrmmer GUI 2.21.0 does not save the interface selection correctly for USB and UART

LurkingKiwi
Associate II

I am having to program a unit via UART, and every time I open the STM32CubeProgrmmer GUI the interface selector shows J-Link/Flasher.

It remembers if I choose ST-Link.

If I manually edit the "interface=" entry in config.properties to 2, STM32CubeProgrmmer opens with UART selected.

On exit, the "interface=" entry is rewritten to 1.

If I select USB as the interface, the "interface=" entry is rewritten to 2, which opens as UART the next time, and then the "interface=" entry is rewritten to 1 on the next exit.

1 REPLY 1
Amine_Jridi
ST Employee

Hello @LurkingKiwi,

Thank you for reporting this. I have submitted a ticket to our team for resolution.

 

Internal ticket number: 227481 (This is an internal tracking number and is not accessible or usable by customers).

 

Thanks,

Amine.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.