2024-03-05 3:01 AM - edited 2024-03-05 3:02 AM
It's been asked before, but the answer has been, "it's not possible as it is not supported on ARM based devices"; eg,
So, is there any plan to make an STM32CubeProgrammer which will run on an ARM-based Linux Host?
It could be quite useful for making a small, portable, standalone programmer ...
Solved! Go to Solution.
2024-03-19 4:52 AM
Hello @Andrew Neil,
This request has already been raised to the dev team, I'll keep you updated on the progress.
Internal ticket number: 176491 (This is an internal tracking number and is not accessible or usable by customers).
Maryem.
2024-03-05 3:03 AM
In the meantime, here are some alternatives (from one of the threads linked previously):
2024-03-19 4:52 AM
Hello @Andrew Neil,
This request has already been raised to the dev team, I'll keep you updated on the progress.
Internal ticket number: 176491 (This is an internal tracking number and is not accessible or usable by customers).
Maryem.
2024-04-25 1:12 AM
Just replying to up the importance of this: our test system uses many, many Raspberry Pis, one to control each board under test and, for whatever reason, OpenOCD (0.12.0-3, latest version from XPack as I write) is not able to flash download to a NUCLEO-U575ZI-Q board reliably (see my post here); I would like to be able to use the "official" ST mechanism on the Raspberry Pi.