2019-06-24 1:57 PM
I am running Windows 7 and v2.1.0 of the STM32CubeProgrammer. It is unable to find connected ST-Link devices (in this instance, an ST-Link/V2, a Nucleo STM32F411RE, and a Nucleo STM32F303RE).
However, if I click the "Firmware Upgrade" button, it is able to find / detect the devices without issue. As well, if I run the older ST-Link Utility v4.50 it is able to detect all of these and connect to the Nucleo boards without issue.
I suspect this is some soft of driver issue on Win7 as the devices are detected on a Win10 laptop without issue as well.
Any ideas?
Cheers,
Martin Z.
2019-06-24 3:30 PM
Most of my system are Win7, so not a specific issue there.
Can find ST-LINK's.
Watch for the default SWD clock, 4000 KHz is too high to connect to an L4 via ST-LINK/V2
2019-06-25 7:06 AM
The issue is with detecting the ST-Link, not with connecting to the target device, so the SWD clock setting doesn't even factor into it.