2021-12-16 10:26 PM
The ST-LINK / V2 programmer is not detected on my PCs.
Before that, when I had a win7 x64 PC with a core i5 processor - STM32CubeProgrammer worked. I currently have a Ryzen 3600 win7 x64. I have installed the latest STM32CubeProgrammer 2.9.0 and am getting "no st-link detected" error. Moreover, through the STM32 ST-LINK Utility, the programmer is detected and works. Everything works through STM32CubeIDE too. I tried all possible driver versions, still no st-link detected. I tried different versions of STM32CubeProgrammer both x64 and x86, still no st-link detected. I tried various USB ports, both USB 2.0 and USB 3.0, tried different ST-LINK / V2 programmers (I have several of them), I even tried on another PC with the same configuration (Ryzen 3600 win7 x64), I still get an error no st-link detected.
Why is that? What else do I need to do to make STM32CubeProgrammer work on my PC?
2021-12-21 12:07 AM
I deleted all ST-LINK linked devices, but still st-link detected.
All versions of windows (7 and 10) I use with Russian localization. As a result, wherever win10 is installed, everything works. Does not work only on windows 7. But at the same time, some previous version of STM32CubeProgrammer definitely worked for me on win7. Perhaps the reason is some kind of win7 update ... Now I have downloaded all available versions of STM32CubeProgrammer and none of them work on win7 ...