STM32CubeProgrammer “Error: Download verification failed�?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-05-11 4:51 AM
Hardware used:
STM32H747I-DISC0 Discovery kit (MB1248-H747I-D02 / A191001982)
Tools used:
STM32CubeProgrammer v2.4.0.
STM32CubeIDE v1.3.1 for code generation
(gnu-tools-for-stm32.7-2018-q2-update_1.0.0.201904181610)
STM32CubeProgrammer gives me an error when I try to program M4 using embedded bootloader. I have no problem programming M7 similarly.
Error:
13:35:23 : Error: Data mismatch found at address 0x08100040 (byte = 0xFF instead of 0xAD)
13:35:23 : Error: Download verification failed
I follow the steps below to access embedded bootloader:
1- Program option bytes on application code(M7) - ( I’m just update BOOT_CM7_ADD0 = 0x1FF0 )
2- Power Off -> Power On
3- Connect the embbeded bootlaoder (After push the Reset Push-Button(B1) Why?? )
STM32CubeProgrammer log:
13:34:59 : STM32CubeProgrammer API v2.4.0
13:34:59 : ST-LINK error (DEV_CONNECT_ERR)
13:35:05 : Serial Port COM52 is successfully opened.
13:35:05 : Port configuration: parity = even, baudrate = 115200, data-bit = 8, stop-bit = 1.0, flow-control = off
13:35:06 : Timeout error occured while waiting for acknowledgement.
13:35:06 : Activating device: OK
13:35:06 : Chip ID: 0x450
13:35:06 : BootLoader protocol version: 3.1
13:35:08 : UPLOADING OPTION BYTES DATA ...
13:35:08 : Bank : 0x00
13:35:08 : Address : 0x5200201c
13:35:08 : Size : 308 Bytes
13:35:08 : UPLOADING ...
13:35:08 : Size : 1024 Bytes
13:35:08 : Address : 0x8000000
13:35:08 : Read progress:
13:35:09 : Data read successfully
13:35:09 : Time elapsed during the read operation is: 00:00:01.136
13:35:22 : Memory Programming ...
13:35:22 : Opening and parsing file: FL_CTRL_CM4.hex
13:35:22 : File : FL_CTRL_CM4.hex
13:35:22 : Size : 4880 Bytes
13:35:22 : Address : 0x08100000
13:35:22 : Erasing memory corresponding to segment 0:
13:35:22 : Erasing internal memory sector 8
13:35:22 : Download in Progress:
13:35:23 : File download complete
13:35:23 : Time elapsed during download operation: 00:00:01.203
13:35:23 : Verifying ...
13:35:23 : Read progress:
13:35:23 : Error: Data mismatch found at address 0x08100040 (byte = 0xFF instead of 0xAD)
13:35:23 : Error: Download verification failed
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-05-12 9:33 AM
Is there anyone who can help me?
Thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-05-19 4:11 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-07-07 2:09 PM
I had the same issue (https://community.st.com/s/question/0D53W00000Bs2G1SAJ/stm32h755-st-bootloader-not-working-on-bank-2)
My solution: Erase the whole chip and than skip flash erase before programming!