cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer erase fails under Linux

Duckpaddle
Associate III

I noticed that the V 2.20 STM32CubeProgrammer erase function doesn't work under Pop_OS!, a Linux distribution.  It does however work on Windows 10.  I don't think this is a logic failure within the STM32CubeProgrammer but some weird interaction with the USB Driver.  Just to be clear I am using STLink on a STM32N6 evaluation board.  Interesting that this function does work on a STM32h747i_disco board.  Another difference is I am using an USB A to USB C cable, but all the other functions work, after erase on the Windows machine.  

I have the erase under Windows workaround but it is a little inconvenient.

 

7 REPLIES 7
Duckpaddle
Associate III

The exact error is: Error: Mass erase operation failed.Please verify flash protection

Ozone
Principal III

Did you check your user is part of the required groups (usually dialout and plugdev) ?

Does the udev rules file cover both ST-Links, which might be different versions ?

Duckpaddle
Associate III

Yes, my user is a member of both groups.  Yes, I am using the same executable V 2.20 for both the N6 and H7 processor.

> Yes, I am using the same executable V 2.20 for both the N6 and H7 processor.

No, that's not what I meant.
The folder /etc/udev/rules.d/ contains text files describing the devices to which the "plugdev" rules apply.
At least on my (Debian-based) distros.
Here an excerpt from "99-jlink.rules" from one of my systems :
ATTR{idProduct}=="1010", ATTR{idVendor}=="1366", MODE="666"
ATTR{idProduct}=="1011", ATTR{idVendor}=="1366", MODE="666"
ATTR{idProduct}=="1012", ATTR{idVendor}=="1366", MODE="666"
ATTR{idProduct}=="1013", ATTR{idVendor}=="1366", MODE="666"
ATTR{idProduct}=="1014", ATTR{idVendor}=="1366", MODE="666"
...
As you see, it lists several product IDs, for different JLink adapter versions in this case.
I think it's at least worth to check both that your ST-Link IDs match.

I don't know Pop-OS, but what I read it is Debian/Ubuntu-based as well, so it should be similiar.

Alternatively, you can try OpenOCD to erase/flash the STM32N6 board, which supports ST-Link as well.

Duckpaddle
Associate III

Thank you for the clarification: 

I will try the OpenOCD, good thought!

 

I used Gemini as an intelligent grep and it said that my 99-jlink.rules file has the rules you suggested:

Yes, your 99-jlink.rules file already contains the exact permissions suggested by the vendor.

Those lines are present in the section defining the permissions for the "[new format]" J-Link Product IDs.

Here is the matching section from the file you provided:

Code snippet
 
...
ATTR{idProduct}=="100f", ATTR{idVendor}=="1366", MODE="666"
ATTR{idProduct}=="1010", ATTR{idVendor}=="1366", MODE="666"
ATTR{idProduct}=="1011", ATTR{idVendor}=="1366", MODE="666"
ATTR{idProduct}=="1012", ATTR{idVendor}=="1366", MODE="666"
ATTR{idProduct}=="1013", ATTR{idVendor}=="1366", MODE="666"
ATTR{idProduct}=="1014", ATTR{idVendor}=="1366", MODE="666"
ATTR{idProduct}=="1015", ATTR{idVendor}=="1366", MODE="666"
...

Your configuration file includes these rules and many others, so no changes are necessary based on that specific suggestion.

I did check to see if the USB id for the STM32N6 board appeared in my 49-stlinkv3.rules and it does: SUBSYSTEMS=="usb", ATTRS{idVendor}=="0483", ATTRS{idProduct}=="3754", \
    MODE="660", GROUP="plugdev", TAG+="uaccess", ENV{ID_MM_DEVICE_IGNORE}="1", \
    SYMLINK+="stlinkv3_%n"

 

So just to reiterate, my STM32CubeProgrammer does connect to the STM32N6 board but fails on erase either mass erase or the erase prior to programming a hex file.

> The exact error is: Error: Mass erase operation failed.Please verify flash protection

I suppose this is not the case, the initial post implies as much.

> Another difference is I am using an USB A to USB C cable, but all the other functions work, after erase on the Windows machine.

And I suppose you have tried different cables. I have heard about such instances occasionally.

> Just to be clear I am using STLink on a STM32N6 evaluation board.  Interesting that this function does work on a STM32h747i_disco board.

Another difference might be the ST-Link firmware version.
Perhaps the version on the N6 eval board requires an update.


By the way, I downloaded the JLink firmware for ST-Links from Segger's website, and converted basically all my onboard ST-Links. Not the least because I use Segger Embedded Studio, which does not support the ST-Link directly (at least the free version I use).

This process is reversible.
If all else fails you could reflash this ST-Link to a JLink, and see if it works fine with different firmware.
AFAIK the CubeProgrammer supports JLinks, but better check before ...