cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer cannot finish installing

RDermenci
Associate II

I am trying to install STM32CubeProgrammer v2.8.0 on my Windows10 (Home x64) computer. I have updated my Java version to 8.301 (64-bit). However, installation process doesn't go further than Step 7 out of 8. There's no "Next" button or something, but just "Quit" button. Even if I wait for minutes, it doesn't change.

What could be the reason for failed installing of STM32CubeProgrammer?

Thanks for help in advance.

P.S. I have had installed STM32CubeIDE v1.7 without any problem.

Ramazan Dermenci

1 REPLY 1
SLemb.1
Associate

When I was trying to install the IDE on Windows10 it gave installation error. All I had to do was move the desktop installation program to C:\ and it worked.