2025-03-10 7:01 AM
I've just noticed that STM32CubeProgrammer (2.19.0) can't see network disk on my Windows 10 PC.
I have also set a folder inside of one of the network disk as favourite folder to rapid access on the left sidebar but, when I click it via STM32CubeProgrammer Explorer it says the path is invalid
The network disk is at X://
2025-03-10 7:10 AM - edited 2025-03-10 7:10 AM
Do you run CubeProgrammer as administrator (elevated)?
2025-03-10 7:10 AM
Yes
2025-03-10 10:59 AM
If it runs under different account (Administrator vs your normal user) it does not see the network shares of the user account. CubeProgrammer normally does not need to run elevated.