2021-12-08 2:54 AM
I am trying to use the STM32CubeProgrammer API to program and read a STM32G491.
so that we can use it in our programming solution. (We write a CRC of the application so that a bootloader can validate it. )
The problem is that the readout of memory does not always work correctly.
I am running the Example1 project with the API.
(On a nucleo-g491RE demo board)
This does a read after a sector erase.
this results in the same data readout as before the sector erase.
Reading 32-bit memory content
Size : 64 Bytes
Address: : 0x08000000
0x08000000 : BBBBAAAA FFFFFFFF FFFFFFFF FFFFFFFF
0x08000010 : FFFFFFFF FFFFFFFF FFFFFFFF FFFFFFFF
0x08000020 : FFFFFFFF FFFFFFFF FFFFFFFF FFFFFFFF
0x08000030 : FFFFFFFF FFFFFFFF FFFFFFFF FFFFFFFF
Flash sector erase ...
Existing specified sectors are erased successfully
Protected sectors are not erased
UPLOADING ...
Size : 64 Bytes
Address : 0x8000000
Read progress:
██████████████████████████████████████████████████ 100%
Data read successfully
Time elapsed during the read operation is: 00:00:00.007
Reading 32-bit memory content
Size : 64 Bytes
Address: : 0x08000000
0x08000000 : BBBBAAAA FFFFFFFF FFFFFFFF FFFFFFFF
0x08000010 : FFFFFFFF FFFFFFFF FFFFFFFF FFFFFFFF
0x08000020 : FFFFFFFF FFFFFFFF FFFFFFFF FFFFFFFF
0x08000030 : FFFFFFFF FFFFFFFF FFFFFFFF FFFFFFFFWhen I read the data with the STM32CubeProgrammer application after this it does read as erased.
So what can I do to get a accurate readout of the memory.