cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer 2.18 BUG on STM32H730

COSEBE
Senior

Hi,

I found a bug on new version 2.18 STM32Cube programmer.

Of course, I have the same problem with the new version of STM32CubeIde 1.17

It looks file STM32_Prog_DB_0x483.xml in \Data_Base folder has changed between versions 2.17 and 2.18

If I use the file STM32_Prog_DB_0x483.xml from the version 2.17 and I replace this file in version 2.18, I can access my STM32H730 device.

We tried it on 2 different computers.

I do not really understand the xml file differences, so I do not know if I can continue to use STM32_Prog_DB_0x483.xml file of version 2.17 with version 2.18 and STM32CubeIDE 1.17

Do you have a workaround ?

Sébastien

15 REPLIES 15

Hi @Maryem 

Do you have any feedback of this problem.

I just looking for a workaround right now.

I cannot develop my firmware for almost 1 month now.

Regards,

Sébastien

Hello @COSEBE ,

 

I've sent you a message. Could you check your DM?

 

Maryem.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Yes, DM is answered

COSEBE
Senior

Hi @Maryem,

Thank you for the patch, everything is working now.

Sébastien

seiran
Associate

I Have the same problem. How to get the patch and how to install it?

Hi Maryem,

I too have a custom board with this issue on this chip. I have upgraded to STM32CubeProgrammer 2.18 and upgraded my STLink V2. I cannot program via STM32cubeIDE as well, but can read target info on CubeProgrammer. Essentially the same as the original post.

What is the fix??

Thanks