cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer 2.10.0 and 2.11.0 External loader bug: if the EL's filename has more tha one dot (one dot only for its extension name) STM32CubeProgrammer goes in error.

Gianluca Costa
Associate II

If the name (filename) of module has more than one dot ( "." ) the STM32CubeProgrammer can list it in the external loder (EL) selection, but when STM32CubeProgrammer tries to use the module it fails (it generates an error).

For example this EL name generates the error: EN25Q40_MT447R2_2.0.0.stldr

the same file renamed into EN25Q40_MT447R2.stldr (removing all dots) works.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Houda GHABRI
ST Employee

Hello @Gianluca Costa,

STM32CubeProgrammer should accept more than one dot in EL file name.

I will raise this issue internally to fix it in future release.

Internal ticket number: 131762 (PS: This is an internal tracking number and is not accessible or usable by customers). 

Houda

View solution in original post

2 REPLIES 2
Andrew Neil
Super User

Always best to avoid any "weirdness" in file (including folder) names

It's an age-old problem:

https://www.avrfreaks.net/comment/1844411#comment-1844411

https://www.avrfreaks.net/comment/2048571#comment-2048571

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Houda GHABRI
ST Employee

Hello @Gianluca Costa,

STM32CubeProgrammer should accept more than one dot in EL file name.

I will raise this issue internally to fix it in future release.

Internal ticket number: 131762 (PS: This is an internal tracking number and is not accessible or usable by customers). 

Houda