2024-05-04 4:33 AM - edited 2024-05-04 2:25 PM
Hello,
Stm32cubeprogrammer installation does not proceed to the final stage, it remains at step 8 and is not completed. I tried the program on three different PCs with administrator rights, the result is the same, the installation does not complete.
Solved! Go to Solution.
2024-05-20 11:51 PM
Hello @Aziz BRIGUI
This is the situation on the PC I use.
I tried installing Windows 10 and Windows 11 on two different PCs without installing any programs, the result did not change, it remains at step 8. I think it might be regional or Windows language related.
2024-05-22 5:58 AM
Hello @Aziz BRIGUI
Let me share an update on the issue.
I tried to make a fresh installation with English (USA) Language Windows 11 and install the program, it was installed without any problems.
My computer's language is Turkish, I added an English language pack to this computer, then I tried the installation again and it was installed without any problems.
Turkish I cannot complete the installation with Windows 11 and Windows 10. I hope you can solve this problem as soon as possible.
2024-08-06 1:41 AM
Thank you very much, @Soner23 . I had the same problem and thanks to you I fixed it.
2024-10-06 12:02 AM
Bende denedim ayni hata aliyorum uzaktan baglanma sansınız var mi
2025-07-05 8:47 AM
Hello everyone, I read the topic from beginning to end, as Mr. Soner said, I was about to lose my mind with these problems...
The computer I use is win 11 pro sp3 Turkish. I added US Eng. language from the language options and installed it without any problems on the first try...