cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 cube programmer - Checksum in automatic mode

RCast.5
Associate

Hi everyone,

In automatic mode, does STM32cubeprogrammer do a "Full Flash memory checksum"?

It does in STM32 ST-Link utility. Of course, the "Full Flash memory checksum" box is checked.

Thank you in advance for your answer

In the log window

STM32 cube programmer

In automatic mode

12:37:22 : Waiting for device n:2...
12:37:29 : Memory Programming ...
12:37:29 : Opening and parsing file: XXXX
12:37:29 : File : XXXX
12:37:29 : Size : 21.56 KB
12:37:29 : Address : 0x08000000
12:37:29 : Erasing memory corresponding to segment 0:
12:37:29 : Erasing internal memory sectors [0 10]
12:37:30 : Download in Progress:
12:37:30 : File download complete
12:37:30 : Time elapsed during download operation: 00:00:00.833
12:37:30 : Verifying ...
12:37:30 : Read progress:
12:37:30 : Download verified successfully
12:37:30 : Please disconnect device n:2 and connect the next...

 

Manualy

12:48:12 : UR connection mode is defined with the HWrst reset mode
12:48:12 : ST-LINK SN : XXX
12:48:12 : ST-LINK FW : XXX
12:48:12 : Board : --
12:48:12 : Voltage : 3.27V
12:48:12 : SWD freq : 4000 KHz
12:48:12 : Connect mode: Hot Plug
12:48:12 : Reset mode : Hardware reset
12:48:12 : Device ID : XXX
12:48:12 : Revision ID : Rev Z
12:48:12 : Debug in Low Power mode is not supported for this device.
12:48:12 : UPLOADING OPTION BYTES DATA ...
12:48:12 : Bank : 0x00
12:48:12 : Address : 0x40022020
12:48:12 : Size : 20 Bytes
12:48:12 : UPLOADING ...
12:48:12 : Size : 1024 Bytes
12:48:12 : Address : 0x8000000
12:48:12 : Read progress:
12:48:12 : Data read successfully
12:48:12 : Time elapsed during the read operation is: 00:00:00.007

12:48:17 : Memory Programming ...
12:48:17 : Opening and parsing file: XXX
12:48:17 : File : XXX
12:48:17 : Size : 21.56 KB
12:48:17 : Address : 0x08000000
12:48:17 : Erasing memory corresponding to segment 0:
12:48:17 : Erasing internal memory sectors [0 10]
12:48:18 : Download in Progress:
12:48:18 : File download complete
12:48:18 : Time elapsed during download operation: 00:00:00.679
12:48:18 : Verifying ...
12:48:18 : Read progress:
12:48:18 : Download verified successfully
12:48:18 : Memory [0x08000000 : 0x08040000] - Checksum : 0x03C012EA

 

STM32 ST Link Utility

In automatic mode

13:02:36 : Starting Automatic Mode...
13:02:36 : Waiting for device N° 1...
13:02:41 : ST-LINK SN : 54FF76067871515408251467
13:02:41 : V2J45S7
13:02:41 : Connected via SWD.
13:02:41 : SWD Frequency = 4,0 MHz.
13:02:41 : Connection mode : Normal.
13:02:41 : Debug in Low Power mode enabled.
13:02:41 : Device ID:0x435
13:02:41 : Device flash Size : 256KBytes
13:02:41 : Device family :STM32L4x3
13:02:41 : Flash programming:
13:02:42 : Memory programmed in 1s and 78ms.
13:02:43 : Full memory checksum calculation..
13:02:43 : Flash memory [0x08000000:0x08040000] Checksum: 0x03BF8556
13:02:43 : Please disconnect device N° 1...

3 REPLIES 3
Maryem
ST Employee

Hello @RCast.5 ,

 

I apologize for the delayed response, 

Currently, STM32CubeProgrammer does not support the "Full Flash memory checksum" feature in automatic mode. This request has already been raised to our development team. I will keep you updated about any progress.

Internal ticket number: 191520 (This is an internal tracking number and is not accessible or usable by customers)

 

Maryem.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hello @Maryem,

I have taken your response into account.

Thank you for your answer, and have a nice day!

Hi @Maryem ,

I would like to ask when this feature is expected to be completed?

This seems to be a very simple feature but it has not been added in the updated version.

 

Best Regards,

Lyon