2024-06-04 2:12 AM
STMicroelectronics ST-LINK GDB server. Version 7.7.0
Copyright (c) 2024, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.16.0
-------------------------------------------------------------------
Log output file: C:\Users\faruk\AppData\Local\Temp\STM32CubeProgrammer_a16684.log
ST-LINK SN : 066EFF534871754867222516
ST-LINK FW : V2J45M30
Board : NUCLEO-F303RE
Voltage : 3.26V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x446
Revision ID : Rev Y
Device name : STM32F302xE/F303xE/F398xx
Flash size : 512 KBytes
Start Address : 8000000
Device type : MCU
Device CPU : Cortex-M4
BL Version : 0x40
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a16684.srec
File : ST-LINK_GDB_server_a16684.srec
Size : 16.75 KB
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 8]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:00.928
Verifying ...
Download verified successfully
Shutting down...
Exit.
I keep getting this error. I didn't get it before, it developed suddenly. it doesn't work in my previous working codes. I made a port change, it didn't change. I did debug update, it didn't happen. I turned the computer off and on, it didn't happen. I deleted the cubeide and reinstalled it, it didn't happen. can someone help me now.
2024-06-18 6:21 AM
Hello @asda
The shutting down message signifies that the CubeProgrammer plug-in did download and verify the binary. Could you share what is the issue you're seeing with this message, are you unable to debug your application ?
Aziz