2024-05-02 05:51 AM
Hi,
I'm having problems entering in DFU mode on Windows using a sensortile.box pro. The board doesn't even show up on device manager howerver using the same board, with the same USB cable, on the same USB port on the same PC running Ubuntu the board enters DFU mode normally. I tried reinstalling CubeProgrammer more than once and also removing and reinstallig drivers but to no avail.
Has anyone had the same problem?
2024-05-20 03:39 AM
Hello @Ig,
I tried an STM32U585 (Since I don't have the exact sensortile board on hand) and it enters DFU mode just fine on Windows. So maybe try to select the driver from CubeProgrammer installation path in Windows ? If you have other DFU hosts (Dfuse for example), try removing them.
Hope this helps,
Aziz
2024-06-11 11:28 AM
Having the same problem, I have two Windows 10 computers, and two SensorTile.Box PRO. Can not get either into DFU.
2024-06-26 12:41 AM