cancel
Showing results for 
Search instead for 
Did you mean: 

SensorTile.box pro not entering DFU mode on Windows

Ig
Associate

Hi,

I'm having problems entering in DFU mode on Windows using a sensortile.box pro. The board doesn't even show up on device manager howerver using the same board, with the same USB cable, on the same USB port on the same PC running Ubuntu the board enters DFU mode normally. I tried reinstalling CubeProgrammer more than once and also removing and reinstallig drivers but to no avail.

Has anyone had the same problem?

3 REPLIES 3
Aziz BRIGUI
ST Employee

Hello @Ig,

I tried an STM32U585 (Since I don't have the exact sensortile board on hand) and it enters DFU mode just fine on Windows. So maybe try to select the driver from CubeProgrammer installation path in Windows ? If you have other DFU hosts (Dfuse for example), try removing them.

Hope this helps,

Aziz


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
gbaker
Associate

Having the same problem, I have two Windows 10 computers, and two SensorTile.Box PRO.  Can not get either into DFU.

zeinebou
Associate

Hello @Ig @gbaker  ,

Did you find a solution? I am facing the same problem.