2021-11-04 03:02 AM
I wanted to connect to my STM32 MCU with STM32CubeProgrammer but forgot to power on the board. The programmers (I had 2 boards with 2 STLINK-v3MINIs connected) were detected but when I connected to one, STM32CubeProgrammer crashed. When powered everything worked fine. Something to look into for next version.
System:
Ubuntu 20.04.1
JRE version: OpenJDK Runtime Environment (9.0_265-b01) (build 1.8.0_265-b01)
Java VM: OpenJDK 64-Bit Server VM (25.265-b01 mixed mode linux-amd64 compressed oops)
STM32CubeProgrammer v2.8.0
STLINK version: V3J7M2