2023-07-18 08:47 AM
Please Never use a popup any where in the app its extremely annoying, use a window I propse you call it "Console" or "LOG " .. oh what do you know you already have one!!!.. so please stop with the popups... also remove the Refresh button Let Connect do both and again upon success or failure please write it to the Console/Log Window
Thanks
2023-07-18 08:53 AM - edited 2023-07-18 08:54 AM
sorry - what you talking about ?
stmProg ....error - or what ?
which cpu ? show screenshot, whats wrong .
2023-07-18 09:09 AM - edited 2023-07-18 09:11 AM
Those pop ups belong in here as log entrys which should be colour coded to red for errors and green for success
and the device refresh is a unecessary step
2023-07-18 09:25 AM
many pics - but still i not know, what you want to do.
is it so difficult to describe ?
2023-07-18 09:32 AM
just 4 pics, very clear and explicit topic/tag forum positioning + description of what i am asking for .. not sure what more you could require
2023-07-18 09:41 AM
>Please Never use a popup
this is your problem ?
or "connection...lost " ? this is a PROBLEM . most times hardware related...
so show your hardware (picture!) not talking about.
2023-07-18 09:44 AM - edited 2023-07-18 09:45 AM
ok you misundestand through the use of the RESET switch and the programming it self these popups arrise, so that is what i am asking for either to stop using them and write those errors to the existing log that the app already has, or provide a litte tick box or something to disable them, then consider doing something similar with the refresh so you dont have to keep clicking refresh each time the board disconnects
2023-07-18 09:50 AM - edited 2023-07-18 09:51 AM
ok, now i understand -- a little bit.
i never see your popups...so we talking in different worlds .
you have a connection problem - eh ? -> so show your hardware (picture!) not talking about.
i my world : connect - program - verify -- ok -- disconnect .
2023-07-18 10:50 AM
Multiple individual pop-up message boxes for Program / Verify phases seems annoying and unnecessary.
Refresh I can see a case for, the OS doesn't always inform and constantly rescanning could potentially delay/stall the application. Occasionally run in to device level lockup with ST-LINK/V3 vs SiLabs/FTDI type serial dongles, and a couple of apps that probe COM ports, and related registry entries.
Device disconnected, got to be a better approach to this.