2025-01-15 9:21 PM - last edited on 2025-01-15 9:33 PM by Tesla DeLorean
Hello,
Do I need to change the version of STM32CubeProgrammer, or is it just an incorrect setting in the .pro file? Please help me fix it. Thank you in advance.
//----------------------------------------------------------------------------------------------------
Environment
ubuntu 22.04
Qt 6.5.3
qmake version 3.1
STM32CubeProgrammer 2.18.0
gcc version 11.4.0
//--------------------------------------------------------------------------------------------------------
qt pro file
QT += core gui
greaterThan(QT_MAJOR_VERSION, 4): QT += widgets
CONFIG += c++17
#DEFINES += QT_NO_VERSION_TAGGING
# You can make your code fail to compile if it uses deprecated APIs.
# In order to do so, uncomment the following line.
#DEFINES += QT_DISABLE_DEPRECATED_BEFORE=0x060000 # disables all the APIs deprecated before Qt 6.0.0
SOURCES += \
main.cpp \
mainwindow.cpp \
stm32downloader.cpp \
upgradeFirmware.cpp
HEADERS += \
mainwindow.h \
stm32downloader.h
FORMS += \
mainwindow.ui
# Default rules for deployment.
qnx: target.path = /tmp/$${TARGET}/bin
else: unix:!android: target.path = /opt/$${TARGET}/bin
!isEmpty(target.path): INSTALLS += target
API_PATH = "/usr/local/STMicroelectronics/STM32Cube/STM32CubeProgrammer"
INCLUDEPATH += $$API_PATH/api/include
DEPENDPATH += $$API_PATH/api/src
DESTDIR = += $$API_PATH/bin
LIBS += -L"/usr/local/STMicroelectronics/STM32Cube/STM32CubeProgrammer/lib" -lCubeProgrammer_API
RESOURCES += \
icon.qrc
//--------------------------------------------------------------------------------------------------------
The error message from QT
:-1: error: /usr/local/STMicroelectronics/STM32Cube/STM32CubeProgrammer/lib/libCubeProgrammer_API.so: undefined reference to `qt_version_tag@Qt_6.6'
:-1: error: /usr/local/STMicroelectronics/STM32Cube/STM32CubeProgrammer/lib/libCubeProgrammer_API.so: undefined reference to `QString::toUcs4_helper(char16_t const*, long long, char32_t*)@Qt_6'
:-1: error: collect2: error: ld returned 1 exit status
:-1: error: [Makefile:371: +=/stm32FirmwareUpgrade] Error 1
//-------------------------------------------------------------------------------------------------------
2025-01-31 1:10 AM - edited 2025-02-03 12:47 AM
Hello @LeonSu,
I managed to reproduce the error you're seeing as well as some other issues with the CubeProgrammer API and Linux. All is logged under Ticket 201804 (This is an internal tracking number not accessible by customers on community).
For now, I'm not finding any workarounds. I will give you an update as soon as anything changes. This will be fixed in a future release.
Aziz
2025-01-31 2:06 PM - edited 2025-01-31 2:07 PM
It looks like the CubeProgrammer API module wants Qt libraries 6.6 but you have 6.5.3.