Associate
March 3, 2023
Solved
Is QSPI-Flash program/read/erase possible via UART bootloader
- March 3, 2023
- 4 replies
- 3064 views
Hi,
is it generally possible to program/read/erase an external connected Flash-Memory (e.g. Quad-SPI-Flash) with STM32CubeProgrammer via USART bootloader?
- I'm using the STM32L496-DISCO board for test.
- External loader MX25R6435F_STM32L496-DISCO selected
- BOOT0 connected to Vdd
- COM1-RX/TX/GND (3.3 V level) connected to MCU USART3 bootloader pins PC10/PC11/GND
With upper configuration MCU-Flash program/read/erase is possible, but no access to Quad-SPI-Flash (address = 0x90000000), see picture.
With selected ST-LINK probe access to Quad-SPI-Flash is possible.
Thanks in advance,
Karsten