2018-01-22 10:51 AM
I'm running Mac OSX 10.9.5
I installed STM32CubeMX.app without problem and it runs fine.
However, when trying to install STM32CubeProgrammer.app it hangs at step 6 of the install program. Running the installer from the command line showed that the installer encountered this error:
Exception in thread 'IzPack - Unpacker thread' java.lang.ClassCastException: java.base/jdk.internal.loader.ClassLoaders$AppClassLoader cannot be cast to java.base/java.net.URLClassLoader
at com.izforge.izpack.installer.unpacker.UnpackerBase.logIntro(UnpackerBase.java:253)
at com.izforge.izpack.installer.unpacker.UnpackerBase.unpack(UnpackerBase.java:285)
at com.izforge.izpack.installer.unpacker.UnpackerBase.run(UnpackerBase.java:242)
at java.base/java.lang.Thread.run(Thread.java:844)
Any workaround for this?
#installer #mac-osx #stm32cubeprogrammerSolved! Go to Solution.
2018-02-02 7:46 PM
FIXED! (With help from this blog post:
http://blueeyes.sakura.ne.jp/2018/01/01/734/
)Install Java 8.
Run this command in a terminal (from the folder holding
SetupSTM32CubeProgrammer-1.0.0.app
:JAVA_HOME=$(/System/Library/Frameworks/JavaVM.framework/Versions/A/Commands/java_home -v '1.8')
./SetupSTM32CubeProgrammer-1.0.0.app/Contents/MacOsSetupSTM32CubeProgrammer-1_0_0_macos
Installs STM32CubeProgrammer.app, which runs OK under Java 9. But won't install under Java 9!
2018-01-23 4:43 AM
Hi Andrew,
can you please provide your java version with 'java -version' in command line.
BR,
Aymen.
2018-01-24 6:07 PM
>$ java -version
java version '9.0.4'
Java(TM) SE Runtime Environment (build 9.0.4+11)
Java HotSpot(TM) 64-Bit Server VM (build 9.0.4+11, mixed mode)
2018-02-01 7:25 PM
OK I've just bought a brand new MacBook Pro, MacOS HighSierra 10.13.3.
Exactly as before. STM32CubeMX installs (but only if you run Terminal in D
ownloads/en.stm32cubeprog/SetupSTM32CubeProgrammer-1.0.0.app/contents/MacOs
and runopen SetupSTM32CubeMX-4_24_0_macos
). Runs OK.But installer for STM32CubeProgrammer hangs on step 6 or 8 of the graphical installer with this thrown exception:
Andrews-MacBook-Pro:~ shep$ /Users/shep/Downloads/en.stm32cubeprog/SetupSTM32CubeProgrammer-1.0.0.app/Contents/MacOs/SetupSTM32CubeProgrammer-1_0_0_macos ; exit;
Command line arguments:
====================
Installation started
Exception in thread 'IzPack - Unpacker thread' java.lang.ClassCastException: java.base/jdk.internal.loader.ClassLoaders$AppClassLoader cannot be cast to java.base/java.net.URLClassLoader
at com.izforge.izpack.installer.unpacker.UnpackerBase.logIntro(UnpackerBase.java:253)
at com.izforge.izpack.installer.unpacker.UnpackerBase.unpack(UnpackerBase.java:285)
at com.izforge.izpack.installer.unpacker.UnpackerBase.run(UnpackerBase.java:242)
at java.base/java.lang.Thread.run(Thread.java:844)
I'm running the latest and greatest for Mac and STM32CubeProgrammer won't even install! I find that strange.
Help!
2018-02-01 7:26 PM
Oh, and my Java environment:
Andrews-MacBook-Pro:MacOs shep$ java -version
java version '9.0.4'
Java(TM) SE Runtime Environment (build 9.0.4+11)
Java HotSpot(TM) 64-Bit Server VM (build 9.0.4+11, mixed mode)
2018-02-02 7:46 PM
FIXED! (With help from this blog post:
http://blueeyes.sakura.ne.jp/2018/01/01/734/
)Install Java 8.
Run this command in a terminal (from the folder holding
SetupSTM32CubeProgrammer-1.0.0.app
:JAVA_HOME=$(/System/Library/Frameworks/JavaVM.framework/Versions/A/Commands/java_home -v '1.8')
./SetupSTM32CubeProgrammer-1.0.0.app/Contents/MacOsSetupSTM32CubeProgrammer-1_0_0_macos
Installs STM32CubeProgrammer.app, which runs OK under Java 9. But won't install under Java 9!
2018-07-10 1:02 PM
I was unable to install with the command listed as it is missing a '/' between 'MacOS' and 'Setup'.
I have added the updated command line that worked correctly for me.
JAVA_HOME=$(/System/Library/Frameworks/JavaVM.framework/Versions/A/Commands/java_home -v '1.8') ./SetupSTM32CubeProgrammer-1.0.0.app/Contents/MacOs/SetupSTM32CubeProgrammer-1_0_0_macos
2020-04-08 11:07 AM
I am also trying to install the MacOS version of the programmer version 2.4.0, and have followed this thread. I got the application installed OK (had to use sudo to write to the Applications directory). My java is version "13.0.1" 2019-10-15. My OS is Mojave 10.14.6
However, when I try and run the programmer, nothing happens, except a slight twitch of the icon bar.
Has anyone succeeded in this installation recently.
Tony
2022-06-01 4:59 AM
I am also have problem install STM32CubeProgrammer v2.10.0 after installation show a error with message ""CubeProgrammer_API or one of its dependencies is missing. Please try reinstalling the program of check your java architecture". I am also already following instruction above. I hope somebody tell Me how to fix it. Thanks