2019-10-22 1:04 PM
I am not able to start STM32CubeProgrammer even installed Oracle JDK 13.0.1 and openjfx:
System: Ubuntu 18.04 VirtualBox on MacOS 10.15:
~$ STM32CubeProgrammer
Error: Could not find or load main class com.st.app.Main
Caused by: java.lang.NoClassDefFoundError: javafx/application/Application
~$ java --version
java 13.0.1 2019-10-15
Java(TM) SE Runtime Environment (build 13.0.1+9)
Java HotSpot(TM) 64-Bit Server VM (build 13.0.1+9, mixed mode, sharing)
2019-10-23 12:26 AM
Hi Jason,
Here is the procedure to get CubeProgrammer working with ubuntu18.04
1- Install OpenJDK 8 :
=> sudo apt install openjdk-8-jre-headless
2- Set OpenJDK 8 as your default Java Runtime Engine :
=> sudo update-alternatives --config java
3- Install OpenJFX
=> sudo apt purge openjfx
=> sudo apt install openjfx=8u161-b12-1ubuntu2 libopenjfx-jni=8u161-b12-1ubuntu2 libopenjfx-java=8u161-b12-1ubuntu2
=> sudo apt-mark hold openjfx libopenjfx-jni libopenjfx-java
and finally don't forget to create stlink and DFU usb rules (described in user manual) to get STM32CubeProgrammer working without "sudo".
BR,
Aymen.
2019-10-24 2:14 PM
The rules files are in /etc/udev/rules.d but still see the STLINK V3 got lost somehow:
Ubuntu18:/etc/udev/rules.d$ ls -l
total 140
-rw-r--r-- 1 root root 619 Oct 24 13:39 49-stlinkv2-1.rules
-rw-r--r-- 1 root root 491 Oct 24 13:39 49-stlinkv2.rules
-rw-r--r-- 1 root root 883 Oct 24 13:39 49-stlinkv3.rules
-rw-r--r-- 1 root root 97 Oct 22 12:10 50-usb-conf.rules
-rw-r--r-- 1 root root 381 Sep 21 11:07 61-msp430uif.rules
-rwxr-xr-x 1 root root 2145 Sep 21 11:07 70-mm-no-ti-emulators.rules
-rw-r--r-- 1 root root 58549 Sep 20 17:18 70-snap.core.rules
-rw-r--r-- 1 root root 705 Oct 14 13:26 70-snap.prospect-mail.rules
-rw-r--r-- 1 root root 669 Oct 14 08:36 70-snap.thunderbird.rules
-rw-r--r-- 1 root root 691 Sep 21 11:05 71-bh-permissions.rules
-rw-r--r-- 1 root root 559 Sep 21 11:06 71-sd-permissions.rules
-rw-r--r-- 1 root root 1814 Sep 21 11:06 71-ti-permissions.rules
-rw-rw-r-- 1 root root 18450 Oct 14 05:03 99-jlink.rules
-rw-r--r-- 1 root root 4286 Sep 21 11:12 99-jlink.rules.O
-rw-r--r-- 1 root root 217 Oct 22 12:10 Readme.txt
-rw-r--r-- 1 root root 5 Oct 22 12:10 version.txt
Ubuntu18:/etc/udev/rules.d$ STM32_Programmer_CLI -l
-------------------------------------------------------------------
STM32CubeProgrammer v2.2.0
-------------------------------------------------------------------
===== DFU Interface =====
No STM32 device in DFU mode connected
===== STLink Interface =====
-------- Connected ST-LINK Probes List --------
ST-Link Probe 0 :
ST-LINK SN : 002200293137510739383538
ST-LINK FW : V3J3M2
-----------------------------------------------
===== UART Interface =====
Total number of serial ports available: 1
Port: ttyACM0
Location: /dev/ttyACM0
Description: STLINK-V3
Manufacturer: STMicroelectronics
Ubuntu18:/etc/udev/rules.d$ STM32_Programmer_CLI -l
-------------------------------------------------------------------
STM32CubeProgrammer v2.2.0
-------------------------------------------------------------------
===== DFU Interface =====
No STM32 device in DFU mode connected
===== STLink Interface =====
Error: No ST-Link detected!
===== UART Interface =====
Total number of serial ports available: 0
2020-02-21 6:51 AM
I confirm this is the only valid procedure to run STM32CubeProgrammer on Ubuntu 18.04
Here is the procedure to get CubeProgrammer working with ubuntu18.04
1- Install OpenJDK 8 :
=> sudo apt install openjdk-8-jre-headless
2- Set OpenJDK 8 as your default Java Runtime Engine :
=> sudo update-alternatives --config java
3- Install OpenJFX
=> sudo apt purge openjfx
=> sudo apt install openjfx=8u161-b12-1ubuntu2 libopenjfx-jni=8u161-b12-1ubuntu2 libopenjfx-java=8u161-b12-1ubuntu2
=> sudo apt-mark hold openjfx libopenjfx-jni libopenjfx-java
2020-03-12 6:39 AM
Hi,
I follow exactly what you wrote but about line 17, I get:
version 8u161-b12-1ubuntu2 for openjfx was not find
Any idea ???
2020-06-07 10:01 PM
Ubuntu 18.04 is now pretty old and a new LTS release is available.
Any chance of making it work with OpenJDK 11?
These openjfx versions are not available on 19.10 and 20.04...
2020-06-15 1:50 PM
Confirms it works. I don't know much about ubuntu but typed it and Voilà! Thanks!
2020-08-06 1:10 PM
Agreed, I can't get this to work with Ubuntu 20.04
I can run the CLI application and connect to the STLINKv3 and see the microcontroller but can't install jfx of hte specified versions
2020-10-12 3:53 AM
I was able to get it to work on Ubuntu 20.04.1 LTS using the Liberica JDK. But I havent thoroughly tested it.
I followed the instructions here to install it: https://stackoverflow.com/a/62746011/848627
You may need to uninstall other openjfx stuff you have installed previously, not sure.
edit: It did managed to do a ST-Link firmware upgrade, and a flash in USB mode (not st-link mode), so presumably it all works as expected.