2020-04-01 08:33 AM
Hi, are there any information's or app-notes available how to use this programmer over CAN bus. I cant find any information which hardware is supported or how make the can hardware on my laptop visible to the programmer.
Thanks for your support!
Solved! Go to Solution.
2020-04-01 08:51 AM
To the best on my knowledge the CAN support in STM32CubeProgrammer is via the STLINK/V3SET boards. The API also has examples.
For the CAN protocol implementation use the following app note, and code a solution for your PC side CAN implementation/drivers
The support costs for third-party CAN implementations is likely too high, and if you have specific hardware/software you're familiar with, implementing the protocol should be straight-forward enough.
2020-04-01 08:51 AM
To the best on my knowledge the CAN support in STM32CubeProgrammer is via the STLINK/V3SET boards. The API also has examples.
For the CAN protocol implementation use the following app note, and code a solution for your PC side CAN implementation/drivers
The support costs for third-party CAN implementations is likely too high, and if you have specific hardware/software you're familiar with, implementing the protocol should be straight-forward enough.
2020-04-02 12:55 AM
Thanks, I ordered a STLINK/V3SET .
Maybe I'll write my own Software as well. Thanks !
2023-10-19 09:44 AM
Hello
If you are developing custom bootloader and planning to use STLINK-V3SET., please email me as I have developed custom Bootloader and not able to connect with STLINK-V3SET. Kindly email me if you are available.
sivakumar.mariappan@electro-flight.com.
Thanks
Siva