2024-01-08 9:33 PM
There is an uninstaller at ~/STMicroelectronics/STM32Cube/STM32CubeProgrammer/uninstaller/uninstaller.jar
But when I java -jar it, it just produce a log then exited, and nothing in the log actually mean anything useful.
I see there is a old post about the same issue, but it never got any further.
As a software product from an actual company, not provide a working uninstaller is unacceptable.
Please fix this or provide a workaround ST.
2024-01-12 7:45 AM - edited 2024-01-12 7:46 AM
Hello, there is a directory named uninstaller containing the uninstaller in the STM32CubeProgrammer install directory ( /usr/local/STMicroelectronics/STM32Cube/STM32CubeProgrammer by default ).
If your system doesn't automatically execute the java .jar program when opening it from a graphical file manager, you will need to start it using the following command (executed in the directory containing the uninstaller program):
$ sudo java -jar uninstaller.jar
Keep in mind, that you need to have Java runtime installed, eg. OpenJDK-JRE
2024-01-12 7:51 AM
Please actually read the post before reply...
As I stated, I already tried invoke the uninstaller.jar, but it didn't do anything other than produce a log which contains nothing useful and no any error.
It's simply the uninstaller do not work
2024-01-12 7:57 AM - edited 2024-01-12 7:58 AM
I apologize, I will try to investigate the issue further.
Can you please link the other related threads that you have mentioned?
2024-01-14 12:19 PM - edited 2024-01-14 12:20 PM
2024-01-16 5:01 PM
2024-01-16 5:03 PM
the installer did not require root access, why the uninstaller needs it?
and the install folder is under my home folder, why it needs root perm. to uninstall?
I haven't try this since there is no any error in the log related to this, if something not work then run with sudo is also a bad bad idea
2024-11-24 10:16 AM
Hi!
I am having the same issue, still not fixed in CubeProgammer 2.17.0.
Have you had any luck uninstalling it?
Thank you!