cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE 1.19.1 + STM32CubeWL build fails on new project: 'ResponseTimeout' member not found

R_JPstudent
Visitor

Hello,

I'm having trouble building a LoRaWAN project targeting the STM32WLE5JCI6. The same error occurs even on a clean, newly created project, which leads me to believe there might be a compatibility issue between the IDE and the software package.

■ The error I'm facing:

../Middlewares/Third_Party/LoRaWAN/Mac/LoRaMac.c: In function 'ProcessRadioRxDone':
../Middlewares/Third_Party/LoRaWAN/Mac/LoRaMac.c:1650:40: error: 'McpsIndication_t' {aka 'struct sMcpsIndication'} has no member named 'ResponseTimeout'

This error indicates that LoRaMac.c is trying to access the ResponseTimeout member of the McpsIndication_t struct, but the corresponding LoRaMac.h file lacks that definition.

■ My setup:

  • Target MCU: STM32WLE5JCI6

  • STM32CubeIDE Version: 1.19.1 (Clean install from the official website)

  • STM32CubeWL Package: Latest version (Installed via the IDE's package manager)

■ Steps I have already taken:

  1. Cleanly reinstalled both STM32CubeIDE and the STM32CubeWL package.

  2. Deleted the old project and workspace, then created a new project from scratch in a new workspace.

  3. The project was generated with default settings, with only the LoRaWAN stack enabled.

■ My findings:

  • The LoRaMac.h file within my new project folder does not contain the definition for the ResponseTimeout member.

  • The latest LoRaMac-node repository on GitHub, however, does include this definition.

■ My question:

Is this a known issue with the combination of the latest STM32CubeIDE and STM32CubeWL package? If you know of a solution, your assistance would be greatly appreciated.

I am using an AI to formulate this question.
Thank you.


1 REPLY 1
Ghofrane GSOURI
ST Employee

Hello @R_JPstudent 

Could you please share your project files ? This will help me better understand your configuration  and assist you more effectively.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.