cancel
Showing results for 
Search instead for 
Did you mean: 

how can i pass step 7 while setup stm32 cube programmer

Gdönm.1
Associate II

when i create this program everything is ok until step7. however i cant pass step 7

and window is below.0693W000008xUekQAE.png

13 REPLIES 13

enabling shortcuts is in step 7 which is shown empty as others have posted. In step 6 the files and drivers are downloaded after the download, I press next and an empty page with only one option "quit" is shown (It is same as the others have posted the screen shot of).

Bkork.1
Associate

0693W00000QNEUUQA5.png 

operating system: windows 10 pro x64

I'm trying to install cubeprogrammer v2.11.0

Can't get past the screen above.

I formatted the computer and it still didn't work.

I tried all of the above answers and it still didn't work.

(the answers above don't work.)

YToks.1
Associate

I had the same issue as Gdönm.1 and i was surfing at the stmcubeprogrammer files and i've found this so i clicked and it worked ! Maybe this could work for you too.0693W00000WIw9AQAT.jpg

Thank you very much, this is the solution, I registered on that forum to say this :D