2021-01-07 7:01 AM
Because I do not have access to the BOOT0 pin (custom board, not eval board) I have used the software method of branching into the bootloader : https://stm32f4-discovery.net/2017/04/tutorial-jump-system-memory-software-stm32/
I have adpted this code for the device (notably bootloader address 0x1FF0 0000)
USART2 physical pins are PA2 and 3
My questions are:
____
logs from Cube
15:59:33:510 : Serial Port COM34 is successfully opened.
15:59:33:511 : Port configuration: parity = even, baudrate = 115200, data-bit = 8, stop-bit = 1.0, flow-control = off
15:59:33:511 : No Init bits value is : 0
15:59:33:511 : Sending init command:
15:59:33:511 : byte 0x7F sent successfully to target
15:59:34:511 : Wait ends after 1 loop, dataready = 0, delay = 1001
15:59:34:511 : Timeout error occured while waiting for acknowledgement.
15:59:34:512 : No response from target received
15:59:34:519 : byte 0x7F sent successfully to target
15:59:34:621 : Wait ends after 1 loop, dataready = 0, delay = 100
15:59:34:621 : Timeout error occured while waiting for acknowledgement.
15:59:34:621 : No response from target received
15:59:34:621 : Error: Activating device: KO. Please, verify the boot mode configuration and check the serial port configuration. Reset your device then try again...
Any help is appreciated, thank-you!
Solved! Go to Solution.
2021-01-07 11:25 AM
I think you're going to need to write your own loader in the front few KB of the L151
Using a protocol like X-Modem allows more commonly available terminal applications to push new binaries into the device.
2021-01-07 9:50 AM
If you jump into the bootloader directly after reset, or in a state where clocks/peripherals are at their reset values, the bootloader will listen on all support interfaces and will respond to the first one that sends a message. No additional configuration needed.
If you have a scope, I would look at the signals on the line. Possibly try using a lower baud rate as well.
Next time just add a debug port to your board. It's a headache without one and a productivity drain.
2021-01-07 11:22 AM
Got anything chattering on USART1? Or other used pins?
Doesn't it expect USART2 signals to be on PD5/PD6?
2021-01-07 11:25 AM
I think you're going to need to write your own loader in the front few KB of the L151
Using a protocol like X-Modem allows more commonly available terminal applications to push new binaries into the device.
2021-01-08 12:06 AM
Thanks so much for the rapid replies.
I am not sure where the issue is. I am using the L152RD eval project IAP (which was TrueStudio) then I imported it into CubeIDE. Therefore I have 2 projects, my app code and the IAP. The final objective is to be able to flash the app code when it is broken. Originally my design was a 2 app combo with a jump from IAP to the app if upgrade not needed. That was before I realized that the IAP/ymodem upgrade is not what I need. Now I am using the IAP app just to test the upgrade mechanism via USART2. It took quite a while to modify the original project to get USART2 up and running (basically a call to clock it was missing because the original code uses USART1). Therefore I have a skeleton IAP app that can do I/O through USART2. Now I need the bootloader part so that it can dialog with any standard flash tool (CubeProgrammer, st-link, whatever).
There is no possibility to "add a debug port" because this is a qualified finished production board.
Yes Tesla, but my debug/interface port is on PA2 and 3. (USART2 has several mappings).
It is possible but unlikely that the issue could be that the eval true studio code conversion to cube caused a problem (my app uses the HAL interface and the eval project uses the StdPeriph_Driver.
Other musings:
#if defined(USE_HAL_DRIVER)
HAL_RCC_DeInit();
#endif /* defined(USE_HAL_DRIVER) */
#if defined(USE_STDPERIPH_DRIVER)
RCC_DeInit();
#endif /* defined(USE_STDPERIPH_DRIVER) */
sufficient to remove previous clock settings and therefore default to HSI?
My next steps;
I'll let you know ...
Thanks for your help
2021-01-08 7:10 AM
I think you're missing what @Community member is saying.
> Yes Tesla, but my debug/interface port is on PA2 and 3. (USART2 has several mappings).
This was doomed at the start. The USART2 bootloader isn't on PA2/PA3, it doesn't matter if those pins can be used by USART2 if the bootloader isn't listening on them.
> this is a qualified finished production board.
Didn't anyone qualify the bootloader interface?
2021-01-08 7:18 AM
Tesla DeLorean I think you are right about the PD5/6 pins and this is why the "standard" bootloader is not talking to CubeProgrammer. I have provoked bootloader execution by clearing the flash and pulling the BOOT0 pin high (in this case it is available but in final package it is not). And still no COM on USART2 PA2/3. I think the pre-installed bootloader only listens to PA10/11 USART1 and PD5/6 USART2.
For making my own bootloader I see 2 options, IAP/y-modem protocol and stm32 bootloader x-modem. Do you have a recommendation? And is the host side software available also or is this limited to teraterm settings?
Thanks again for your help!
2021-01-08 7:22 AM
TDK Yes you are right, therefore I will have to code a bootloader myself that talks to those pins until we do a re-design of our board. Thanks again for your help!
2021-01-08 7:23 AM
"Didn't anyone qualify the bootloader interface?" lol, I am a software guy, you know what hardware designers say "Fix it in software!"
2021-01-08 8:52 AM