2021-01-07 7:31 PM
Launching the app from the bin directory doesn't work either and there are no errors in the terminal. It just silently fails. I believe part of the problem is the update to version 2.6.0 which uses its own bundled JRE. Perhaps there is a conflict with the OpenJDK (Amazon Corretto) JRE installed on my machine. However, it is necessary to have JRE on my machine to run STM32CubeMX and STM32CubeIDE.
I tried to download the previous version (2.5.0) and run that. It does not launch either, however, there are errors in the terminal.
~ % /Applications/STMicroelectronics/STM32Cube/STM32CubeProgrammer/STM32CubeProgrammer.app/Contents/MacOs/bin/STM32CubeProgrammer ; exit;
Exception in Application start method
java.lang.reflect.InvocationTargetException
at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at sun.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:62)
at sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.lang.reflect.Method.invoke(Method.java:498)
at com.sun.javafx.application.LauncherImpl.launchApplicationWithArgs(LauncherImpl.java:389)
at com.sun.javafx.application.LauncherImpl.launchApplication(LauncherImpl.java:328)
at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at sun.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:62)
at sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.lang.reflect.Method.invoke(Method.java:498)
at sun.launcher.LauncherHelper$FXHelper.main(LauncherHelper.java:873)
Caused by: java.lang.RuntimeException: Exception in Application start method
at com.sun.javafx.application.LauncherImpl.launchApplication1(LauncherImpl.java:917)
at com.sun.javafx.application.LauncherImpl.lambda$launchApplication$1(LauncherImpl.java:182)
at java.lang.Thread.run(Thread.java:748)
Caused by: javafx.fxml.LoadException:
file:/Applications/STMicroelectronics/STM32Cube/STM32CubeProgrammer/STM32CubeProgrammer.app/Contents/MacOs/bin/STM32CubeProgrammer!/fxml/MainWindow.fxml:217
at javafx.fxml.FXMLLoader.constructLoadException(FXMLLoader.java:2601)
at javafx.fxml.FXMLLoader.loadImpl(FXMLLoader.java:2579)
at javafx.fxml.FXMLLoader.loadImpl(FXMLLoader.java:2441)
at javafx.fxml.FXMLLoader.loadImpl(FXMLLoader.java:3214)
at javafx.fxml.FXMLLoader.loadImpl(FXMLLoader.java:3175)
at javafx.fxml.FXMLLoader.loadImpl(FXMLLoader.java:3148)
at javafx.fxml.FXMLLoader.loadImpl(FXMLLoader.java:3124)
at javafx.fxml.FXMLLoader.loadImpl(FXMLLoader.java:3104)
at javafx.fxml.FXMLLoader.load(FXMLLoader.java:3097)
at com.st.app.Main.start(Main.java:38)
at com.sun.javafx.application.LauncherImpl.lambda$launchApplication1$8(LauncherImpl.java:863)
at com.sun.javafx.application.PlatformImpl.lambda$runAndWait$7(PlatformImpl.java:326)
at com.sun.javafx.application.PlatformImpl.lambda$null$5(PlatformImpl.java:295)
at java.security.AccessController.doPrivileged(Native Method)
at com.sun.javafx.application.PlatformImpl.lambda$runLater$6(PlatformImpl.java:294)
at com.sun.glass.ui.InvokeLaterDispatcher$Future.run(InvokeLaterDispatcher.java:95)
Caused by: java.lang.RuntimeException: java.lang.reflect.InvocationTargetException
at javafx.fxml.JavaFXBuilder$ObjectBuilder.build(JavaFXBuilderFactory.java:278)
at javafx.fxml.FXMLLoader$ValueElement.processEndElement(FXMLLoader.java:763)
at javafx.fxml.FXMLLoader.processEndElement(FXMLLoader.java:2823)
at javafx.fxml.FXMLLoader.loadImpl(FXMLLoader.java:2532)
... 14 more
Caused by: java.lang.reflect.InvocationTargetException
at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at sun.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:62)
at sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.lang.reflect.Method.invoke(Method.java:498)
at sun.reflect.misc.Trampoline.invoke(MethodUtil.java:72)
at sun.reflect.GeneratedMethodAccessor1.invoke(Unknown Source)
at sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.lang.reflect.Method.invoke(Method.java:498)
at sun.reflect.misc.MethodUtil.invoke(MethodUtil.java:276)
at javafx.fxml.JavaFXBuilder$ObjectBuilder.build(JavaFXBuilderFactory.java:270)
... 17 more
Caused by: java.lang.UnsatisfiedLinkError: Can't load library: /Library/Java/JavaVirtualMachines/amazon-corretto-8.jdk/Contents/Home/jre/lib/libjfxwebkit.dylib
at java.lang.ClassLoader.loadLibrary(ClassLoader.java:1820)
at java.lang.Runtime.load0(Runtime.java:810)
at java.lang.System.load(System.java:1088)
at com.sun.glass.utils.NativeLibLoader.loadLibraryFullPath(NativeLibLoader.java:201)
at com.sun.glass.utils.NativeLibLoader.loadLibraryInternal(NativeLibLoader.java:94)
at com.sun.glass.utils.NativeLibLoader.loadLibrary(NativeLibLoader.java:39)
at com.sun.webkit.WebPage.lambda$static$0(WebPage.java:133)
at java.security.AccessController.doPrivileged(Native Method)
at com.sun.webkit.WebPage.<clinit>(WebPage.java:132)
at javafx.scene.web.WebEngine.<init>(WebEngine.java:881)
at javafx.scene.web.WebEngine.<init>(WebEngine.java:868)
at javafx.scene.web.WebView.<init>(WebView.java:273)
at javafx.scene.web.WebViewBuilder.build(WebViewBuilder.java:60)
... 27 more
Exception running application com.st.app.Main
2021-01-08 3:49 AM
Hi @ARive.2 ,
To use STM32CubeProgrammer 2.5.0 :
OpenJDK (Amazon Corretto) is not recommended .You can use Zulu 8 instead as mentioned in this link :
https://community.st.com/s/question/0D53W00000KonaSSAR/stm32cubeprogrammer-zulu8-jre-recommended .
For STM32CubePRogrammer 2.6.0 :
Being in this path : /Applications/STMicroelectronics/STM32Cube/STM32CubeProgrammer/STM32CubeProgrammer.app/Contents/MacOs/bin/ , can you plz try to launch CubeProgrammer using one of this two commands
1- ./STM32CubeProgrammer
2- ../../../jre/bin/java -jar STM32CubeProgrammer
3- Try with CubeProgrammer_CLI and tell me if it is OK
Please try these commands and send me the log file .
Houda
2021-01-08 4:38 AM
Houda - thanks for the reply. I tried v2.6.0.
1 - Failed with the following error:
./STM32CubeProgrammer
./STM32CubeProgrammer
,????
chdir /Applications/STMicroelectronics/STM32Cube/STM32CubeProgrammer/STM32CubeProgrammer.app/Contents/MacOs/bin/.
current dir /Applications/STMicroelectronics/STM32Cube/STM32CubeProgrammer/STM32CubeProgrammer.app/Contents/MacOs/bin
Exec error: No such file or directory2 -
bin % ../../../jre/bin/java -jar STM32CubeProgrammer
zsh: no such file or directory: ../../../jre/bin/java3 - CLI appears to work.
./STM32_Programmer_CLI
-------------------------------------------------------------------
STM32CubeProgrammer v2.6.0
-------------------------------------------------------------------
Usage :
STM32_Programmer_CLI.exe [command_1] [Arguments_1][[command_2] [Arguments_2]...]
Generic commands:
........
2021-01-08 6:00 AM
Hi @ARive.2 ,
Thanks for your feedback.
When you are trying these commands are you already placed under this path ?Applications/STMicroelectronics/STM32Cube/STM32CubeProgrammer/STM32CubeProgrammer.app/Contents/MacOs/bin/
regards,
Houda
2021-01-08 6:32 AM
Yes. I also just removed Corretto and installed Zulu JDK instead. Here is what I see now.
$ java -version
openjdk version "1.8.0_275"
OpenJDK Runtime Environment (Zulu 8.50.0.53-CA-macosx) (build 1.8.0_275-b01)
OpenJDK 64-Bit Server VM (Zulu 8.50.0.53-CA-macosx) (build 25.275-b01, mixed mode)
$ pwd
/Applications/STMicroelectronics/STM32Cube/STM32CubeProgrammer/STM32CubeProgrammer.app/Contents/MacOs/bin
$ java -jar STM32CubeProgrammer
zsh: killed java -jar STM32CubeProgrammer