2021-07-06 6:02 AM
On the host the card is connected correctly and is being seen by STM32CubeProgrammer (v.2.6.0). On VM upon connection it recieves just the same drivers (the same ID etc), but Programmer doesn't see it at all. It is still somehow available by Putty, but that's not what needed.
2021-07-14 5:24 AM
Hello @IK.4
Can you please tell which OS you are using ?For the debug interface is it DFU , STlink?
Houda
2021-07-14 10:11 PM
Good day, @Houda GHABRI
Thanks for your reply. OS is Win10x64, debug interface is STlink.
Somehow I managed to resolve the problem, the cause of which was the fact that USB redirection doesn't passthrough the device to VM correctly during a connection using Horizont Client. Meanwhile the connection via VMWare Workstation uses standard VMWare passthrough of USB devices, so they work correctly in VM.