2022-03-01 10:14 AM
When trying to connect:
When trying the same thing on a different PC (works on 3 different PCs, doesn't work on 3 other PCs). with the same IC it connects and programs with no issues.
I checked the SW version of Cube programmer, on the 3 PCs that it worked they had versions v2.2.0, v2.6.0 and v2.9.0. The PCs that did not work all had versions v2.9.0.
Someone suggested I check what Java version is installed on the PCs. They all have(working and not working):
java -version
java version "1.8.0_321"
Java(TM) SE Runtime Environment (build 1.8.0_321-b07)
Java HotSpot(TM) 64-Bit Server VM (build 25.321-b07, mixed mode)
I also checked what version of Drivers was beeing used all PCs are using the same version:
I am not sure what else could be different between the different PCs that could be causing such an error, any help would be appreciated.
Thank you
Andre Allain
2022-03-01 10:30 AM
Different on PCs is USB port chipsets and drivers. Too cables connectors maybe differ.
2022-03-01 10:53 AM
The same cable was used accross all PCs.
Also tried multiple ports, front panel and rear. Always with the same results.
One more thing, Once the IC is programmed Serial communication thru Tera term is possible accross all PCs, but still unable to connect to STM Cube programmer on certain PCs
Thank you
Andre
2022-03-03 7:10 AM
We found a work around by using a Type-C USB3.0 hub between the PC and the IC.
I would be very appreciative If some one could explain why this happens.
Thank you.
Andre