cancel
Showing results for 
Search instead for 
Did you mean: 

GETID command not acknowledged

Rsrma.1
Associate III

Hi everyone,

I'm writing my own bootloader for STM32f407VG, in the start address of flash memory. But getting problem GetID command is not acknowledged. I've attached a log also.

10:49:19:443 : RTS low
  10:49:19:443 : DTR low
  10:49:19:443 : Serial Port ttyUSB1 is successfully opened.
  10:49:19:444 : Port configuration: parity = none, baudrate = 9600, data-bit = 8,                     stop-bit = 1.0, flow-control = off
  10:49:19:444 : No Init bits value is : 0 
  10:49:19:444 : Sending init command: 
  10:49:19:444 : byte 0x7F sent successfully to target
  10:49:19:461 : Wait ends after 1 loop, dataready = 1, delay = 9
  10:49:19:461 : Received response from target: 0x79
  10:49:19:462 : Activating device: OK
  10:49:19:462 : Board       : --
  10:49:19:462 : Sending GetID command and its XOR:
  10:49:19:463 : byte 0x02 sent successfully to target
  10:49:19:463 : byte 0xFD sent successfully to target
  10:49:19:475 : Wait ends after 1 loop, dataready = 1, delay = 6
  10:49:19:475 : Received response from target: 0x79
  10:49:19:483 : Received 4 data bytes from target : 0x01041379
  10:49:19:483 : Chip ID: 0x413 
  10:49:19:483 : Sending Get command and its XOR:
  10:49:19:483 : byte 0x00 sent successfully to target
  10:49:19:483 : byte 0xFF sent successfully to target
  10:49:19:498 : Wait ends after 1 loop, dataready = 1, delay = 16
  10:49:19:498 : Received response from target: 0x79
  10:49:19:498 : Received 1 data bytes from target : 0x0b
  10:49:19:498 : size of bytes in the response: 11
  10:49:19:514 : Received 13 data bytes from target
  10:49:19:514 : Full received response: 0b31000102112131446373829279
  10:49:19:514 : BootLoader protocol version: 3.1
  10:49:19:515 : byte 0x11 sent successfully to target
  10:49:19:515 : byte 0xEE sent successfully to target
  10:49:19:614 : data sent successfully to target: 0x0800000008
  10:49:19:628 : byte 0x00 sent successfully to target
  10:49:19:629 : byte 0xFF sent successfully to target
  10:49:19:642 : Device Read Unprotect requested
  10:49:19:642 : Received 1 data bytes from target : 0x00
  10:49:19:642 : Received 1 data bytes from target : 0x00
  10:49:19:642 : Received 1 data bytes from target : 0x91
  10:49:19:643 : Sending read unprotect command and its XOR:
  10:49:19:643 : byte 0x92 sent successfully to target
  10:49:19:643 : byte 0x6D sent successfully to target
  10:49:19:658 : Wait ends after 1 loop, dataready = 1, delay = 15
  10:49:19:659 : Received response from target: 0x79
  10:49:19:659 : Received response from target: 0x79
  10:49:19:665 : Sending init command: 
  10:49:19:665 : byte 0x7F sent successfully to target
  10:49:20:649 : Wait ends after 1 loop, dataready = 1, delay = 986
  10:49:20:650 : Received response from target: 0x79
  10:49:20:664 : Reconnection after RDU OK !
  10:49:20:664 : Checking access to flash after RDU !
  10:49:20:664 : byte 0x11 sent successfully to target
  10:49:20:664 : byte 0xEE sent successfully to target
  10:49:20:760 : data sent successfully to target: 0x0800000008
  10:49:20:782 : byte 0x00 sent successfully to target
  10:49:20:782 : byte 0xFF sent successfully to target
  10:49:20:796 : Sending GetID command and its XOR:
  10:49:20:796 : byte 0x02 sent successfully to target
  10:49:20:796 : byte 0xFD sent successfully to target
  10:49:20:797 : Received response from target: 0x00
  10:49:20:797 : Error: GETID command not acknowledged!
  10:49:20:797 : Reemission of GetID command
  10:49:20:797 : Sending GetID command and its XOR:
  10:49:20:797 : byte 0x02 sent successfully to target
  10:49:20:797 : byte 0xFD sent successfully to target
  10:49:20:797 : Received response from target: 0x00
  10:49:20:797 : Error: GETID command not acknowledged!
  10:49:20:797 : Reemission of GetID command
  10:49:20:798 : Sending GetID command and its XOR:
  10:49:20:798 : byte 0x02 sent successfully to target
  10:49:20:798 : byte 0xFD sent successfully to target
  10:49:20:798 : Received response from target: 0x91
  10:49:20:798 : Error: GETID command not acknowledged!
  10:49:20:798 : byte 0x11 sent successfully to target
  10:49:20:798 : byte 0xEE sent successfully to target
  10:49:20:894 : data sent successfully to target: 0x0800000008
  10:49:20:905 :  UART PORT CLOSE 
  10:49:20:976 : Disconnected from device.
  10:49:20:979 : RTS low
  10:49:20:979 : DTR low
  10:49:20:979 : Serial Port ttyUSB1 is successfully opened.
  10:49:20:979 : Port configuration: parity = none, baudrate = 9600, data-bit = 8,                     stop-bit = 1.0, flow-control = off
  10:49:20:979 : No Init bits value is : 0 
  10:49:20:979 : Sending init command: 
  10:49:20:979 : byte 0x7F sent successfully to target
  10:49:20:985 : Wait ends after 1 loop, dataready = 1, delay = 7
  10:49:20:985 : Received response from target: 0x79
  10:49:20:995 : Activating device: OK
  10:49:20:995 : Board       : --
  10:49:20:995 : Sending GetID command and its XOR:
  10:49:20:995 : byte 0x02 sent successfully to target
  10:49:20:996 : byte 0xFD sent successfully to target
  10:49:21:001 : Wait ends after 1 loop, dataready = 1, delay = 6
  10:49:21:001 : Received response from target: 0x79
  10:49:21:017 : Received 4 data bytes from target : 0x01041379
  10:49:21:017 : Chip ID: 0x413 
  10:49:21:017 : Sending Get command and its XOR:
  10:49:21:017 : byte 0x00 sent successfully to target
  10:49:21:017 : byte 0xFF sent successfully to target
  10:49:21:033 : Wait ends after 1 loop, dataready = 1, delay = 16
  10:49:21:033 : Received response from target: 0x79
  10:49:21:033 : Received 1 data bytes from target : 0x0b
  10:49:21:033 : size of bytes in the response: 11
  10:49:21:049 : Received 13 data bytes from target
  10:49:21:049 : Full received response: 0b31000102112131446373829279
  10:49:21:049 : BootLoader protocol version: 3.1
  10:49:21:049 : byte 0x11 sent successfully to target
  10:49:21:049 : byte 0xEE sent successfully to target
  10:49:21:149 : data sent successfully to target: 0x0800000008
  10:49:21:171 : byte 0x00 sent successfully to target
  10:49:21:171 : byte 0xFF sent successfully to target
  10:49:21:189 : Device Read Unprotect requested
  10:49:21:189 : Received 1 data bytes from target : 0x00
  10:49:21:189 : Received 1 data bytes from target : 0x00
  10:49:21:189 : Received 1 data bytes from target : 0x91
  10:49:21:189 : Sending read unprotect command and its XOR:
  10:49:21:190 : byte 0x92 sent successfully to target
  10:49:21:190 : byte 0x6D sent successfully to target
  10:49:21:203 : Wait ends after 1 loop, dataready = 1, delay = 16
  10:49:21:203 : Received response from target: 0x79
  10:49:21:203 : Received response from target: 0x79
  10:49:21:204 : Sending init command: 
  10:49:21:204 : byte 0x7F sent successfully to target
  10:49:22:185 : Wait ends after 1 loop, dataready = 1, delay = 985
  10:49:22:185 : Received response from target: 0x79
  10:49:22:195 : Reconnection after RDU OK !
  10:49:22:195 : Checking access to flash after RDU !
  10:49:22:195 : byte 0x11 sent successfully to target
  10:49:22:195 : byte 0xEE sent successfully to target
  10:49:22:295 : data sent successfully to target: 0x0800000008
  10:49:22:315 : byte 0x00 sent successfully to target
  10:49:22:315 : byte 0xFF sent successfully to target
  10:49:22:329 : Sending GetID command and its XOR:
  10:49:22:329 : byte 0x02 sent successfully to target
  10:49:22:329 : byte 0xFD sent successfully to target
  10:49:22:329 : Received response from target: 0x00
  10:49:22:329 : Error: GETID command not acknowledged!
  10:49:22:329 : Reemission of GetID command
  10:49:22:329 : Sending GetID command and its XOR:
  10:49:22:330 : byte 0x02 sent successfully to target
  10:49:22:330 : byte 0xFD sent successfully to target
  10:49:22:330 : Received response from target: 0x00
  10:49:22:330 : Error: GETID command not acknowledged!
  10:49:22:330 : Reemission of GetID command
  10:49:22:330 : Sending GetID command and its XOR:
  10:49:22:330 : byte 0x02 sent successfully to target
  10:49:22:330 : byte 0xFD sent successfully to target
  10:49:22:330 : Received response from target: 0x91
  10:49:22:330 : Error: GETID command not acknowledged!
  10:49:22:330 : byte 0x11 sent successfully to target
  10:49:22:330 : byte 0xEE sent successfully to target
  10:49:22:429 : data sent successfully to target: 0x0800000008

I'm receiving the GetID command and sending the response as below.

       uint8_t id_size = 0x01;
	
       uart_write(ACK_BYTE);
       uart_write(id_size);
       uart_write(DEVICE_ID_MSB);
       uart_write(DEVICE_ID_LSB);
       uart_write(ACK_BYTE);

1 ACCEPTED SOLUTION

Accepted Solutions
Rsrma.1
Associate III

I think I've figured out the problem, this was happening because I've not written the read memory execution carefully. After correcting this problem now it's working.

View solution in original post

5 REPLIES 5
MM..1
Chief II

Seems your code isnt executed, what debug stop? , is code on github?

Rsrma.1
Associate III

I've debug it, it's going inside that function and other data is passing.

Rsrma.1
Associate III

I think I've figured out the problem, this was happening because I've not written the read memory execution carefully. After correcting this problem now it's working.

Ok and is your code based on an open source?

Yes, OpenBL.