2024-02-16 10:06 AM
STM32CubeProgrammer v2.15
I'm having the same issue identified in the following post in the latest (as of now) version of STM32CubeProgrammer: https://community.st.com/t5/stm32cubeprogrammer-mcus/flashing-elf-with-stm32cubeprogrammer-flashes-garbage-before/td-p/154225
Can that discussion be re-opened or an update provided here?
2024-02-16 11:43 AM
I don't think it's actually closed to new input, but probably helps to start a new thread
@Houda GHABRI @Nawres GHARBI @STOne-32
Not actually garbage, but .ELF header data, not sure if it keys on extension, case, or magic patterns..
2024-02-16 3:30 PM - edited 2024-02-16 3:31 PM
[removed]
2024-02-16 5:59 PM
It was marked as solved so I just wanted to make sure there was an "open" thread.
2024-02-16 6:39 PM
@Jon Enz Which toolchain produced your .elf file?
2024-02-20 4:29 AM
Hello @Jon Enz ,
For now, I can't reproduce the issue you're seeing with .elf files generated by CubeIDE or EWARM. When relocating an application for an STM32L476 for example, there is a segment in the beginning of the flash, however, this segment has nothing to do with .ELF overhead. I suspect it has to do with jumping to the main application, since removing it will prevent the relocated app from running properly.
As for this thread : https://community.st.com/t5/stm32cubeprogrammer-mcus/flashing-elf-with-stm32cubeprogrammer-flashes-garbage-before/td-p/154225. What I noticed when opening the attachment by @Rami Rosenbaum(using multiple elf parsers/viewers) is that the elf extension overhead is indeed pointed to by a load type segment in the program/segment headers.
That's the part interpreted by CubeProgrammer (and several other tools), and usually that's not the case in elf files, here's an example elf compiled with EWARM (with a relocated app).
So as stated by @Pavel A. & @Tesla DeLorean ,we need to know the toolchain you're using in order to investigate further. Attaching the .ELF file could also be helpful.
Thanks in advance,
Aziz
2024-02-21 5:14 AM
The toolchain used to generate the file was ARM GNU 10-2020-q4-major. I can confirm that loading the .hex file shows the data starting at the correct location.
Unfortunately I cannot share the project files directly, but I was able to create a reduced project that produces the same result. The .elf and .hex files are in the build directory of the attached file. You can re-run the build using the following commands.
Configure:
cmake -B build -DCMAKE_TOOLCHAIN_FILE=toolchain-embedded-arm.cmake -G "MinGW Makefiles" -DCMAKE_BUILD_TYPE:STRING=Debug
Build:
cmake --build build --target ELF-TEST.elf