cancel
Showing results for 
Search instead for 
Did you mean: 

Error: failed to download Segment[0]

JPark.20
Associate II

HI, ST

Im trying to fw update using MFC Tool, STM32_Programmer_CLI.exe.

first, i checked that the fw download operation was completed using Terminal.

so, I makeed the mfc tool in the way the terminal works in the background and checked the fw download works, but it doesn't work well.

this is the output on Debug message(using TRACE()):

[command : STM32_Programmer_CLI.exe -c port=usb1 -d C:\TEST\TEST.bin 0x08000000]

​   -------------------------------------------------------------------

            STM32CubeProgrammer v2.5.0          

   -------------------------------------------------------------------

USB speed  : Full Speed (12MBit/s)

Manuf. ID  : STMicroelectronics

Product ID : STM32 BOOTLOADER

SN     : 205530724352

FW version : 0x011a

Device ID  : 0x0470

Device name : STM32L4Rxxx/STM32L4Sxxx

Flash size : 2 MBytes (default)

Device type : MCU

Device CPU : Cortex-M4

Memory Programming ...

Opening and parsing file: TEST.bin

 File     : TEST.bin

 Size     : 645823 Bytes

 Address    : 0x80000000 

Erasing memory corresponding to segment 0:

Not flash Memory : No erase done

Download in Progress:

 0%

Error: failed to download Segment[0]

Error: failed to download the File

​---------------------------------------------------------------------------------------------------------------------------------------

it doesn't seem to be working from erasing memory before updating. (likewise, '--skipperase')

I appeciate any comment or suggestions

thanks you!!​

1 ACCEPTED SOLUTION

Accepted Solutions
Pavel A.
Evangelist III

Indeed, 0x80000000 is not flash memory (should it be 0x08000000 ?)

--pa

View solution in original post

2 REPLIES 2
Pavel A.
Evangelist III

Indeed, 0x80000000 is not flash memory (should it be 0x08000000 ?)

--pa

yes! im fool!!!!!!!

thanks you Pavel!!!