cancel
Showing results for 
Search instead for 
Did you mean: 

Error: Data mismatch found at address 0x080031A0 (byte = 0xFF instead of 0x80)

travel2moon
Associate

Hi, 

I got the NUCLEO-L433RC-P and just make default build and flash it but i got the data mismatch error:

Error: Data mismatch found at address 0x080031A0 (byte = 0x37 instead of 0x80)

any idea? 

 08:12:39 : STM32CubeProgrammer API v2.16.0 | Windows-64Bits
08:12:44 : UR connection mode is defined with the HWrst reset mode
08:12:44 : ST-LINK SN : 066CFF484971754867143738
08:12:44 : ST-LINK FW : V2J45M31
08:12:44 : Board : NUCLEO-L433RC-P
08:12:44 : Voltage : 3.25V
08:12:44 : SWD freq : 4000 KHz
08:12:44 : Connect mode: Normal
08:12:44 : Reset mode : Software reset
08:12:44 : Device ID : 0x435
08:12:44 : Revision ID : Rev Z
08:12:44 : Debug in Low Power mode is not supported for this device.
08:12:45 : UPLOADING OPTION BYTES DATA ...
08:12:45 : Bank : 0x00
08:12:45 : Address : 0x40022020
08:12:45 : Size : 20 Bytes
08:12:45 : UPLOADING ...
08:12:45 : Size : 1024 Bytes
08:12:45 : Address : 0x8000000
08:12:45 : Read progress:
08:12:45 : Data read successfully
08:12:45 : Time elapsed during the read operation is: 00:00:00.009
08:12:55 : MASS ERASE ...
08:12:55 : Mass erase successfully achieved
08:12:56 : UPLOADING ...
08:12:56 : Size : 1024 Bytes
08:12:56 : Address : 0x8000000
08:12:56 : Read progress:
08:12:56 : Data read successfully
08:12:56 : Time elapsed during the read operation is: 00:00:00.011
08:13:01 : Memory Programming ...
08:13:01 : Opening and parsing file: motodock.bin
08:13:01 : File : motodock.bin
08:13:01 : Size : 12.64 KB
08:13:01 : Address : 0x08000000
08:13:01 : Download in Progress:
08:13:01 : File download complete
08:13:01 : Time elapsed during download operation: 00:00:00.345
08:13:01 : Verifying ...
08:13:01 : Read progress:
08:13:01 : Error: Data mismatch found at address 0x080031A0 (byte = 0x37 instead of 0x80)
08:13:01 : Error: Download verification failed
08:13:02 : RUNNING Program ...
08:13:02 : Address: : 0x08000000
08:13:02 : Warning: The core is locked up
08:13:02 : Start operation achieved successfully

1 ACCEPTED SOLUTION

Accepted Solutions
travel2moon
Associate

Please disregard this report, this is not ST board issue, it is due to wrong battery power to system connect. 

thanks,

View solution in original post

1 REPLY 1
travel2moon
Associate

Please disregard this report, this is not ST board issue, it is due to wrong battery power to system connect. 

thanks,