2025-01-17 7:57 AM - edited 2025-01-17 7:58 AM
Ive been trying to use the FDCAN systembootloader from a stm32H757XI, in the past i managed to use the CAN systembootloader from a stm32f405RE succcesfully.
But im getting> nothing , i tried with 125 and 250Kbauds, CAN connceted to PH14 and PH13
Is FDCAN systembootloader compatible with STLINKV3+CubeProgrammer?
Solved! Go to Solution.
2025-01-21 6:57 AM
@Javier1 wrote:Is FDCAN system bootloader compatible with STLINKV3+CubeProgrammer?
Apparently not - see your other thread:
(a limitation of the ST-Link V3 rather than the bootloader itself)
2025-01-21 6:57 AM
@Javier1 wrote:Is FDCAN system bootloader compatible with STLINKV3+CubeProgrammer?
Apparently not - see your other thread:
(a limitation of the ST-Link V3 rather than the bootloader itself)