cancel
Showing results for 
Search instead for 
Did you mean: 

2.17 still broken dual bank STM32F767ZG

arro239
Senior

I appreciate that something has been changed in this are - I see sector numbering is being different (strange but at least different)

But in the end of the day DFU upload is still broken

 

erasing sector 0005 @: 0x08020000 done
erasing sector 0006 @: 0x08040000 done
erasing sector 0007 @: 0x08060000 done
erasing sector 24786 @: 0x08080000 done
Download in Progress:
±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±± 0%
  2%  4%  6%  8% 10% 12% 14% 16% 18% 20% 22% 24% 26% 28% 30% 32% 34% 36% 38% 40% 42% 44% 46% 48% 50% 52% 54% 56% 58% 60% 62% 64% 66% 68% 70% 72% 74% 76% 78% 80% 82% 84% 86% 88% 90% 92% 94% 96% 98% 100%

File download complete
Time elapsed during download operation: 00:00:21.193



Verifying ...


Read progress:
±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±± 50%
  2%  4%  6%  8% 10% 12% 14% 16% 18% 20% 22% 24% 26% 28% 30% 32% 34% 36% 38% 40% 42% 44% 46% 48% 50% 52% 54% 56% 58% 60% 62% 64% 66% 68% 70% 72% 74% 76% 78% 80% 82% 84% 86% 88% 90% 92% 94% 96% 98% 100%

Error: Data mismatch found at address  0x08080000 (byte = 0x00 instead of 0x49)


Error: Download verification failed

if it helps feel free to test using rusefi.bin file from https://rusefi.com/build_server/rusefi_bundle_proteus_f7.zip

1 REPLY 1
FBL
ST Employee

Hello @arro239 

Thank you for reporting this issue. A new internal ticket 188198 is reported to address DFU upload process.

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL