cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer issue with West flash command

It's the first time I encounter this issue so I'm not familiar with it. It happens with the command "west flash". The problem started after upgrading Zephyr to v3.6.0. Prior to that it was working. Any hints are appreciated!

usage: stm32cubeprogrammer [-h] [-d DIR] [-r RUNNER] [--skip-rebuild] [--domain DOMAIN] [-H] [--board-dir DIR] [--gdb GDB] [--openocd OPENOCD] [--openocd-search DIR]
                           [--elf-file FILE] [--hex-file FILE] [--bin-file FILE] [--erase] [-O TOOL_OPT] --port PORT [--frequency FREQUENCY] [--reset-mode {sw,hw,core}]
                           [--conn-modifiers CONN_MODIFIERS] [--cli CLI] [--use-elf]
stm32cubeprogrammer: error: argument --reset/--no-reset: ignored explicit argument 'hw'

xavierpachecoeaton_0-1722863370555.png

 

0 REPLIES 0