2022-09-14 07:02 AM
I am editing a device tree for my custom board generated by Cube MX. My TF-A .dts folder does not contain any information about QUADSPI which is used for serial flash memory, so should I add a node for quadspi and a child node for flash or I should only edit peripherals generated by CubeMx which are sections like these:
/* USER CODE BEGIN peripheralX */
/* USER CODE END peripheralX */
I am a little confused, can you help me with this? Thank you in advance.
2022-09-27 06:51 AM
Hi @Gencay,
I'm surprise .. QUADSPI is a boot device properly handle in CubeMX.
You get proper node in TF-A DT ( ev1 board example ):
&qspi {
pinctrl-names = "default";
pinctrl-0 = <&quadspi_pins_mx>;
status = "okay";
/* USER CODE BEGIN qspi */
reg = <0x58003000 0x1000>, <0x70000000 0x4000000>;
#address-cells = <1>;
#size-cells = <0>;
flash0:mx66l51235l@0 {
compatible = "jedec,spi-nor";
reg = <0>;
spi-rx-bus-width = <4>;
spi-max-frequency = <108000000>;
#address-cells = <1>;
#size-cells = <1>;
};
/* USER CODE END qspi */
};
QUADSPI internal peripheral - stm32mpu
QUADSPI device tree configuration - stm32mpu
Could you please elaborate further ?
Olivier