2021-07-07 11:10 PM
It comes as surprise to us that the x-cube-display module cannot be enabled on anything else rather than a G0 based MCU.
why can't it be used for other nucleo boards?
2021-07-08 02:39 AM
@dsamm
Hello x-cube-display is an implementation example using X-NUCLEO-GFX01M1 with NUCLEO-G071RB. To date, it does not cover all other Nucleo compatible with X-NUCLEO-GFX01M1.
For the other compatible NUCLEO, you need to adapt the code.
2021-07-08 02:41 AM
Hello @dsamm,
I added STM32CubeMX topic for your post, this will increase its chance to be reviewed by our CubeMx team.
So, our CubeMx team will take in charge to answer you.
Imen
2021-07-08 02:43 AM
@Laurent VERA , the x-cube-display has been defined to be a reusable module, hence it should be possible to include and use it with the other STM32XX MCUs
Unfortunately, it cannot be enabled as per screenshot to work with other MCUs. ( the option is not selectable in CubeIDE )
can you provide a solution?
2021-07-08 02:46 AM
ok, but please recommend a way this driver can be added and used with other stm32 nucleo boards.
2021-07-08 02:46 AM
@Laurent VERA (ST Employee) , the x-cube-display has been defined to be a reusable module, hence it should be possible to include and use it with the other STM32XX MCUs
Unfortunately, it cannot be enabled as per screenshot to work with other MCUs. ( the option is not selectable in CubeIDE )
2021-07-16 06:55 AM
Hi @dsamm and sorry for the delayed reply on this.
I shared your request internally with CubeMX team for review.
Thanks
Imen