2018-11-16 06:13 AM
Hi,
I need create UDP server on STM32F407 with PHY DP83848 in RMII mode. I started with CubeMx, but it support only LAN8720 in this mode.
What is the solution?
Thank you.
Peter
2018-11-19 12:37 AM
Hi @Peko
Thanks for the feedback it will be fixed for the 5.1.0
2018-11-20 12:09 AM
Hi,
the actual version is 4.27. When you plan to release version 5.1.0 ?
What are the differences between LAN8720 and DP83848 in RMII mode?
Peter
2020-01-06 10:31 PM
Hi @Nawres GHARBI
I have tried release version 5.5.0 and this issue still exists. I can see DP83848 as a dropdown option in MII mode only, and LAN8720 as an option in RMII mode only. I am using DP83848 in RMII mode. When do you expect this to be fixed?
@Peko Did you resolve this? Would you be willing to share your CubeMX project and/or code changes?
Matthew.