2021-11-02 3:54 PM
After spending some time debugging my project, I was able to narrow my problem down to this and reproduce it as follows:
assert_failed() at main.c:197 0x80002a0 HAL_NVIC_SetPriority() at stm32l4xx_hal_cortex.c:192 0x80006fe HAL_InitTick() at stm32l4xx_hal_timebase_tim.c:49 0x800030e HAL_RCC_OscConfig() at stm32l4xx_hal_rcc.c:482 0x8000a7a SystemClock_Config() at main.c:124 0x800022c main() at main.c:79 0x80001d8
Solved! Go to Solution.
2023-09-21 6:53 AM
Hi,
am facing the same issue with HAL_InitTick(TICK_INT_PRIORITY); function
is it fixed?
2024-06-06 1:44 PM
I don't think it's fixed as it's now 2024 and I get the same problem on the STM32WB55 :(
2024-06-10 5:44 AM
Hello ,
This issue was detected and reported internally.
Internal ticket number: 183790 (This is an internal tracking number and is not accessible or usable by customers).
Thanks.
Mahmoud
2024-06-10 5:53 AM
Thank you, please can you let me know when this is fixed or any possible workaround? I'm working on a customer project that needs this working soon
Regards
Andrew